• RE: Information Conifrm

    Hi,

    Thanks for using AD9739A. 

    The eval kit does not contain any CD. The software needed to evaluate the evaluation board is available online. ACE is used for SPI communication while DPG Lite is for generating and playing of data vector to DAC.

    ACE: Analysis…

  • AD9119 clocking with ADF4350

    Figure 148 in AD9119 datasheet shows a possible signal chain for the clock path base on ADF4350 PLL usage.

    Figure 22 in ADF4350 datasheet shows the PLL output stage.

    In my opinion, biasing is missing on the ADF4350 side since its output stage do not…

  • AD9739: FPGA selection

    Since AD9739 supports input data rates from 1.6 GSPS to 2.5 GSPS using dual
    LVDS data ports, what host processor can we use to send data to AD9739 and how
    to connect the host processor for example a FPGA with AD9379? Could you please
    provide a…

  • 助力坛友消灭零回复,8种精美礼品等您选!更有价值100的京东卡哦

    各位组员,赚积分、拿奖品的机会来了哦~

    • 解答以下问题,即可获取积分。若果你的回复被标记为“正确答案”、“有用答案”,你的积分就会蹭蹭的往上涨哦~ps.积分=免费礼品,看看你的积分可以兑换什么吧?→带上你的积分,换取你的专属礼品吧
    • 即日起,解答以下问题,跟帖附上您解答的问题链接,活动结束后,回答问题最多的组员,将获得一张价值100元的京东E卡一张。

    • 即日起,解答以下问题,跟帖附上您解答的问题链接,即可在以下奖品中任选一件哦~ps.请提前完善您的个人资料,方便版主邮寄…
  • 助力坛友,共同消灭零回复!

    各位坛友,赚积分的机会来了哦~

    解答以下问题,即可获取积分。若果你的回复被标记为“正确答案”、“有用答案”,你的积分就会蹭蹭的往上涨哦~

    ps.积分=免费礼品,看看你的积分可以兑换什么吧?→带上你的积分,换取你的专属礼品吧

    放大器产品问题:

    AD8336负过冲

    基于AD9865芯片的宽带载波模块设计原理图

    AD8655带宽问题

    ad711的offset null如何使用

    官网没有spice模型怎么解决

    AD8015跨阻放大器,输出信号问题

    是否存在工艺问题

    运放驱动高压M…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • AD9739/7 - Which bits are the MSB in the LVDS interface?

    Looking at the data sheet for the AD9739, I couldn't find any place that explicitly says which side of the LVDS interface contains the MSB.  In other words, is the DB0[0] pin MSB, or is it DB0[13]?  

    If I missed that in the datasheet, please let me…