Hello Viny,
Sorry for the delayed response. No, this capacitor is not necessary. It would help if you were connecting to something with non-zero common mode voltage.
Hello Viny,
Sorry for the delayed response. No, this capacitor is not necessary. It would help if you were connecting to something with non-zero common mode voltage.
尊敬的ADI工程师您好:
AD9737A这款DAC芯片,datasheet上写到模拟输出差分电阻为70欧,我的需求是:输出差分对的N端接一个无源滤波电路,P端接一个无源滤波电路,每个滤波电路特征阻抗都是50欧,请问怎么阻抗匹配?
AD9737A这款芯片配什么时钟芯片,datasheet里提到的ADICLK914频率到达7.5G,而AD9737A要求DACCLK输入范围1.6G—2.5G??怎么用呢?
Sorry for the delay to answer you. It is best to follow the start-up sequence, then set register 0x08 = 0x02. You will need to choose a DAC clock that is far from the 1st Nyquist signal and the 2nd Nyquist image. You will generate your signal in the 1st…
hi,
When i use AD9737A FMC board, i find out that it is just AC-couple from 5MHz to 300MHz. However, i would like to use it by DC-couple because my band-width is from zero to 200MHz. So, how can i modify the EVAL-AD9737A-FMC-EBZ component? I wonder if…
Hi,
Thanks for using AD9739A.
The eval kit does not contain any CD. The software needed to evaluate the evaluation board is available online. ACE is used for SPI communication while DPG Lite is for generating and playing of data vector to DAC.
ACE: Analysis…
Many of our high-speed DACs in that speed range use JESD204B interface which introduces more latency than LVDS. However, if you consult the HIGH-speed DAC product selection guide, you will see a few options beyond the LTC2000, such as AD9737A, AD9739A…
Can you check if the enable pin of U1 - pin 10 is low.
There are two options to talk to ad9737a - FMC SPI or PIC18F24 SPI.