FAQ
您好,
Hello Ms./Mr. ,
从AD9717数据表来看,有重定时器的功能可以对相位进行调整,但是只有最低90°的分辨率,远远不够我的设计要求。
From the data sheet of AD9717, the function of retimer can adjust the phase, but only the minimum resolution of 90° is far from my design requirements.
我想知道AD9717是否有相位控制功能…
Hello Ms./Mr. ,
From the data sheet of AD9717, the function of retimer can adjust the phase, but only the minimum resolution of 90° is far from my design requirements.
I wonder if AD9717 has phase control function? Similar to the phase control word…
Is it possible to create sinusoidal wave using AD9717? If so, how? The DPG Palette on the evaluation board software has an example simple sine generator, but the page is blank. Would appreciate any guidance.
Thanks
1) Does the AD9717 support the power supply configuration: AVDD = 3.3V, CVDD = 3.3V, DVDD = 1.8V, DVDDIO = 1.8V?
2) What is the absolute maximum ratings for DCLKIO?
Hello,
Does AD9717 support next power supply configuration: AVDD = 3.3V, CVDD = 3.3V, DVDD = 1.8V, DVDDIO = 1.8V?
Does "Strap DVDD to DVDDIO at 1.8 V" mean "connect DVDD and DVDDIO pins together on the PCB if DVDD = 1.8V and DVDDIO = 1.…