• AD9716

    We are attempting to use the following circuit to produce a single ended voltage ramp on the output:

         The circuit is based on the circuit used in the AD9716 .  The configure set as

        da_res=1,

        da_cs=0,

        da_sdio=1,

        da_sclk=0,

        da_clko=18.432MHz…

  • AD9716 Full-scale Current Accuracy

    Hello team;

    We are setting AD9716 Full-scale Current as following: enable the internal on-chip 16k ohm Rset; Vref=1V; by which we can get a full-scale current=32* Vref/ Rset=2mA. While by test we found the current is only 1.6mA instead of 2mA. Is this…

  • Pin compatibility between AD9716 and AD9116.

    Hello

    I have a question about pin compatibility between AD9116 and AD9716, from our customer.
    By the datasheet it looks like that these two devices has same package and function of pins.
    He wants to confirm because the data sheet diagram was wrong before…

  • AD9716 - Logic Levels at AVDD=3.3V, DVDD=1.8V, DVDDIO=1.8V, CVDD=1.8V

    I am planning on using  the AD9716 with the following power supply voltages:

    AVDD=3.3V,
    DVDD=1.8V,
    DVDDIO=1.8V,
    CVDD=1.8V

    Can you please provide the digital specification for this power supply
    combination?

     

    Here are the required input specifications…

  • dynamic performance of AD9716 and AD9116 while supplying 1.8V to AVDD

    Hello, I have a question about dynamic performance of AD9716 and AD9116 while supplying 1.8V to AVDD.
    Could you give me the following parameters ?
     - Output Settling Time to 0.1%
     - Output Rise Time (10% to 90%)
     - Output Fall Time (10% to 90%)

    Thanks,

    y_s…

  • AD9176: ACE could not find AD9176-FMC-EBZ

    Hello,

    Our customer has trouble in evaluating AD9176.
    He is trying to do the "DC TEST MODE", he connects PC and AD9716-FMC-EBZ using a USB cable, without ADS8-V1EBZ.
     
    The device manager finds AD9176-FMC-EBZ but the ACE software could not find it…

  • RE: DAC选型

    输出可调的电压范围是多少啊?怎么样的可调发?你要明确你的需求。AD9716你看看符合你的要求不?

  • Should I connect to ground the CMLI, CMLQ, FSADJI and FSADJQ pins?

    Should I connect to ground the CMLI, CMLQ, FSADJI and FSADJQ pins?

    I'm setting the following AD9716 registers with the following values?
    Reg    Bin    Hex
    0x04 10000000 80
    0x05 00000000 00
    0x07 10000000 80
    0x08 00000000 00

     

  • AD971X Digital Specifications at 1.8V

    I am planning on using the AD9716 with the following power supplies DVDD=1.8V, DVDDIO=1.8V, CVDD=1.8V, AVDD=3.3V

    The data sheet does not quote input threshold parameters for either the Data Clock input or Input Data for these power supply conditions…