• AD9715 latency

    Hi,

    how can I make the DAC latency known and deterministic?

    I also need that the latency does not vary in time.

    Thanks a lot.

    Alberto

  • RE: TxDAC Two Singles vs. One Dual

    Thanks Larry, I missed the AD9715 in my parametric search. I was sorting on TxDAC under the features parameter but the AD9715 doesn't have that listed. It looks like a perfect fit for my application.

  • AD971x CML resistor value

    The AD971x daatsheet states that the internal CML resistor can be adjusted from 250 Ohm to 1 kOhm.

    However, Figure 102 shows a variation from 300 to 1100 Ohm. Which one should I consider for the calculation of the output common model level?

    Thanks

  • AD971x self-calibration

    Is it mandatory to write the 32 coefficients to device for the calibration to take effect?

    Thanks

    Alberto

  • RE: AD9761 and AD9763

    The AD9115 and AD9715 are 10 bit dual 125MSPS worth looking at.

    Someone from the HDMI group needs to address the AD9883.

    Thanks,

    Larry

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • AD9717 and AD9117 CML Pins

    What is the purpose of the CMLI and CMLQ pins on the AD9717 and AD9117 DAC famlies and where do they need to be connected?

  • DAC Calibration

    Some high speed DAC have options for auto-calibration. Why and when should I use this option?