• AD9714 frequency response

    The output current is 2mA and with 500 Ohms gives 1V output. Normally DACs have a 20mA output and 50 Ohms. There is no mention of the settling time of frequency response for this part.

  • RE: AD9715 latency

    There is information in the datasheet regarding making the timing deterministic. Please see the "Estimating the Overall DAC Pipeline Delay" section of the datasheet. There is a slight update in process needed for this section which I have copied and corrected…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • AD9717 and AD9117 CML Pins

    What is the purpose of the CMLI and CMLQ pins on the AD9717 and AD9117 DAC famlies and where do they need to be connected?

  • DAC Calibration

    Some high speed DAC have options for auto-calibration. Why and when should I use this option?