您好。很抱歉,没有完全满足您要求的器件。ADC请参考AD9626,AD9230。 但是是差分输入,输入信号幅值也需要调理。DAC可以参考AD9706,AD9742等,是电流输出的DAC
您好。很抱歉,没有完全满足您要求的器件。ADC请参考AD9626,AD9230。 但是是差分输入,输入信号幅值也需要调理。DAC可以参考AD9706,AD9742等,是电流输出的DAC
Looking at the forum for hints on an issue I am having with a design, I found this message:
https://ez.analog.com/message/216361?commentID=216361#comment-216361
I am troubleshooting a board where AD9707 is used and the designer supplied AVDD wit 3.3V…
The AD9706 matches the precision and DAC update rate you desire, and is probably the closest we have to what you need. Its interface is a parallel CMOS interface.
I'm obviously missing something fundamental with figure 89 of the AD970x data sheet - if REFIO is driving 1V to the noninverting input of the op amp, it appears V_iouta will always be >1V; isn't this outside of its compliance range?
Can you…
Hi Andre -
Series terminators are a good idea for the AD9706 data input signals. Ideally they should be close to the signal source and have a value of 25 ohms.
Thank,
Larry
I’m using AD9707 with AVDD=1.8V, CLKVDD=2.5V and DVDD=3.3V power supply according to data sheet that, at pag. 30, states:
“The analog and digital sections of the AD9704/AD9705/AD9706/AD9707 have separate power supply inputs (AVDD and DVDD) that can…
AD693 |
AD5410 |
AD5412 |
AD5420 |
AD5422 |
AD5735 |
AD5755 |
AD5755-1 |
AD5737 |
AD5757 |
AD5421 |
AD421 |
AD5758 |
AD7569 |
AD7669 |
AD7868 |
AD7869 |
AD5593R |
AD5592R |
AD5940 |
AD5941 |
AD7293 |
AD7294-2 |
AD7292 |
AD5590 |
AD7294 |
L… |
Some high speed DAC have options for auto-calibration. Why and when should I use this option?