• 关于AD9704的应用问题

    请问,需要输出40MHZ占空比50%的0-5V幅值调制信号,AD9704+运放的方式能否实现?

  • AD9704问题

    AD9704输入变化,输出不变,量到的REFIO和时钟都正常,但是封装画错,中间的焊盘接地没画,影响转化吗?电路图见附件。

  • SPICE model for AD9704

    Hi

    Is there any spice model for AD9704?

    Regards

    Srikanth Kacchu

  • AD9704问题

    How much is the full-scale current output current of AD9704 in the working mode of 1.8V power supply? Is the principle the same as the working mode of 3.3V? How to adjust thefull-scale current output current ?

  • AD9704 output not consistent

    Hello,

    I am trying to use 2 AD9704 chips to provide inputs to an IQ modulator. Each needs to provide a 1V p-p signal. I added load resistors (IOUTA, IOUTB, QOUTA, QOUTB all have resistors to GND) on the outputs to generate this swing. I am able to do so…

  • About AD9704 full-scale current outputs

    How much is the full-scale current output current of AD9704 in the working mode of 1.8V power supply? Is the principle the same as the working mode of 3.3V? How to adjust thefull-scale current output current ?

  • AD9704: Adjusting common mode output voltage

    Hello,

    I'm trying to use two AD9704 DACs with an IQ modulator. I've attached my schematic below. I added 50ohm resistors between the IOUTA and IOUTB signals of each DAC to GND and am seeing voltages (relative to GND) between 0 and 0.1V based on the input…

  • AD9704 - "powers up in a state that leaves the DAC output nonfunctional".

    I am currently designing an upgrade to existing equipment that needs an additional DAC. I was going to use the AD9704 but when the datasheet was updated from Rev. B to Rev. C in September this year, the following was added in the "Reference Operation…

  • RE: IBIS model for AD9708

    Hi -

    We have an ibis model for the AD9704 which you can use here.

    Thanks

  • RE: AD9705数模转换器外围电路问题,请协助解决。

    你好,我用AD9704,电路图和以上接法差不多,不知道为什么不转换。

    REFIO电压正常,时钟也正常