• AD9697 ADC Samples are zero

    I have the AD9697 (single adc version of the dual adc AD9695). I'm using ADI's linux kernel driver (the ad9208 family driver). I have it configured for L=4, S=1, F=1, K=32, M=2, 16 bits per sample, 16 bit converter resolution, 0 control bits  Fs…

  • AD9697 JESD problem

    I have AD9697, Kintex 7 and AD9528 for clocking. AD9528 works with SI570 (100 MHz base).
    AD9528 gives me  clocks:

    1000 Mhz - for AD9697

    250 Mhz - Ref CLK (for  Kintex)

    31.25 Mhz - SysRef  (for AD9697 and Kintex).

     

    I setup AD9697:

    N'=16, N=14, L=4, M=1, F=1, CS…

  • AD9697 and Kintex 7 SYNC problem

    I have AD9697, Kintex 7 and AD9528 for clocking. AD9528 works with SI570 (100 MHz base).

    AD9528 gives me 2 clocks 1200 MHz (OUT0 and OUT 13) for ADC and FPGA.

    Alsow AD9528 gives m2  2 clocks 120 MHz (OUT2 and OUT 3) for ADC and FPGA for SYS_REF. Additional clk…

  • AD9697 datasheet rev 0 error?

    Hello,

    Is there errors on AD9697 rev0 datasheet (page 65)?

    and page 83:

    Best regards,

    Mlfvr

  • AD9697 Output Configurations for N΄ = 16

    Hi all,


    Our customer is confused by the "lane rate" or "serial lane rate" calculated.


    In the datasheet 65 page,

    Example Setup 1—Full Bandwidth Mode

    • Output serial lane rate:

    • 6.5 Gbps per lane (L = 4).

    • 13 Gbps per…

  • AD9697 and Kintex 7 JESD connection problem

    I have AD9697, Kintex 7 and AD9528 for clocking. AD9528 works with SI570 (100 MHz base).
    AD9528 gives me 2 clocks 1200 MHz (OUT0 and OUT 13) for ADC and FPGA.

    Alsow AD9528 gives m2  2 clocks 120 MHz (OUT2 and OUT 3) for ADC and FPGA for SYS_REF. Additional…

  • AD9697 Zero IF mode and Alias Protected Bandwidth

    We would like to use the AD9697 as the digitizer for an Oscilloscope. This means we need flat band pass response from DC up to the 80% of the bandwidth we want to use, and rejection of alias frequency components above the cut off frequency. We wish to…

  • Missing samples while capturing signal via custom board with ad9697 and ads8v1 capture board

    First of all, we have provided with source codes of ad9695 eval board to be used with ACE gui. We modified those source codes to use ACE and eval capture board ads8v1 together with our custom board designed with ad9697. As far as we read, except for power…

  • RE: What would be the best FDA for AD9690-500

    You can try using the AD9697. it has a lower VCM than the AD9690.

  • RE: AD9695 DC power

    With one channel off, you would be around 60% of total power. You can check out the AD9697 for comparison. This is the single channel version of the AD9695. 

    You can refer to the memory map registers 0x0008 and 0x0002 to disable/power down one channel…