• How is the AD9683 unique?

    How is the AD9683 unique?

     

    Yes, the AD9683 is the only single channel ADC with 14-bit resolution that runs
    greater than 200MSPS (it runs up to 250MSPS) w/ JESD204B outputs. 

  • Does the AD9683 support a smaller package size

    With fewer inputs, does the AD9683 support a smaller package size?

     

    Yes, the AD9683 is available in a 32-lead QFN (5mm2). Most competitive
    offerings are in 40-lead or larger packages.

  • Is there an additional data capture required in order to evaluate the AD9683?

    Is there an additional data capture required in order to evaluate the AD9683?

     

    Yes, it requires the high speed ADC data capture card called HSC-ADC-EVALDZ. 

    http://www.analog.com/en/analog-to-digital-converters/ad-converters/products/ev…

  • AD9250 to AD9683 migration

    Hello Everyone, 

    As a part of an evaluation project, I would like to use AD9683 ( on its FMC evaluation board). However I could not find any project or and library element with name AD9683. 

    My plan is to modify AD9250 to AD9683 as a component and then…

  • AD9683 dev board FMC pinout

    Hello Everybody, 

    Looking into the Schematic of AD9683 development board ad9683_final_schematic_02_040310c.pdf I see this:

    And looking into the schematic of the recommended host FPGA board HSC-ADC-EVALEZ schematic file, sch_hadv6fmc01d.pdf I see the following…

  • AD9683 eval boards

    Hello All,

    I see that there is a picture of an eval board including AD9683-250 in the link below: 

    https://wiki.analog.com/_detail/resources/eval/ad9683_jumpers.jpg?id=resources%3Aeval%3Aad9683-170ebz_ad9683-250ebz_ad6677ebz

    Does this board exist somewhere…

  • AD9683 dev board (with FMC connector) design files

    Hello,

    I hope that everyone is doing great.

    I am writing to ask where I can find design files (schematic, layout, BOM) of the AD9683 dev-board with FMC connector.

    Here (https://wiki.analog.com/resources/eval/ad9683-170ebz_ad9683-250ebz_ad6677ebz) I…

  • FPGA source code AD9683 evaluation

    Hello Everybody,

    Are there any FPGA projects around to evaluate the AD9683 ? Best is something directly could be used on a A10SoC board but anything else is also welcome if A10SoC project is not available. 

    ( For Example  HSC - ADC - EVALEZ is also welcome…

  • RE: Clock adjust AD9683-250EBZ

    please refer to the user guide EVALUATING THE AD9683/AD6677 ANALOG-TO-DIGITAL CONVERTERS [Analog Devices Wiki] for detailed informatioin on how to evaluate the AD9683