• AD9681 balun stage

    Dear ADI engineers, 

    I am using AD9681. 

    The balun stage in AD9681 is MABA-007159-000000 with the frequency region 4.5-3000MHz.

    I would like to work with lower frequency. Could I change this balun stage to another one?

    If possible. Could you recommend me…

  • AD9681 Offset Error

    Hi

    AD9681 Offset Error is +0.21%FSR(typ).

    AD9681 input range is 2Vpp.

    So Offset Error is calculated 2Vx0.21/100=+4.2mV

    Is it right?

    Best regards

    N.Kokubo

  • RE: EVAL-AD9681 + HSC-ADC-EVALDZ

    Hi akgulb,

    Thanks for your interest in AD9681. I've requested that the sample code be emailed to you.

    It is for the HSC-ADC-EVALEZ, which has replaced the .HSC-ADC-EVALDZ.

    You should receive the code within a day or so.

    Thanks,

    Doug

  • One lane mode AD9681 HSC-ADC-EVALEZ

    Hello support team,

    I am working with AD9681 + HSC-ADC-EVALEZ. I've already have the HDL code for configure it. 

    But in the code I have, there is only option for two lane mode. 

    Could I ask the HDL code part for one lane mode? 

    Thank you,

    HOANG

  • FPGA source code AD9681 capture board HSC - ADC - EVALEZ

    Hello,

               I work with a set of HSC-ADC-EVALEZ +AD9681. Now my work is to program the FPGA on HSC-ADC-EVALEZ (Virtex 6). But I don't understand how it woks without example. I can't restore source code from .mcs file. Whether is there any source code for…

  • Using AD9681 eval board with ZCU102

    Hello all!

    Does AD9681 have a ZCU102 driver Demo? If so, can share a copy?

    Thanks!

  • AD9681 xilinx ultrascale data capture HDL code.

    Hi. I'm using AD9681.

    I want to capture data with xilinx ultrascale FPGA .

    Is there any HDL code for this?

  • Drive AD9681 single-ended

    Hi

    I'm a DFAE in Japan. Our customer considers driving the AD9681 inputs single-ended. Is it possible? If it is possible, could you please tell me the recommended driver circuit?

    Regards,

    Hiroyuki

  • 关于AD9681是否可被zynq-7020的pl端驱动

    您好:
    我想咨询AD9681是否可以被zynq-7020的PL端驱动(zynq7020的性能是否足够)。我们需要做卫星的探测载荷,由于卫星能源控制严格,我们需要低功耗、多通道(至少8个)、高采样率(~100M)的ADC,目前看中AD9681,但是不知道是否可以被我们的主控芯片ZYNQ-7020使用,如果不可以的话,请问是否有其他类似的能尽量满足我们需求的ADC

  • AD9681 high noise floor

    Hello


    We have a problem with our AD9681-125EBZ board (01-039100, REV B). We are using it with the Digilent Nexys Video FPGA board. When sampling very low power signals, the ADC works as expected. But when sampling signals closer to the full scale, the…