• ad9680

    1. Referring to Figure 1 and Figure 2, I would like to ask whether the R204 resistor in the evaluation board AD9680-1000 has been installed, because it is covered by the transformer, so I can't see clearly. Since J201 is not installed on the evaluation…

  • AD9680-1000 SNR/Nosie Level become worse accidentally

    Hi,

      I use 8 AD9680-1000 in my customer board, so there are 16 AD channels. I use HMC7044 to provide system  and JESE204B clock and use LDO to provide power.  Sometimes, after power up and configure registers, one channels SNR may become worse than usual. In…

  • AD9680 Design

    Hi:

        I'm planning to use AD9680 to develop a reciever system. There's some issues confusing me, can anybody answer my questions?

    1. I found that there are two evaluation boards for AD9680, one named 9680CE04B and another named 9680CE02B. They…

  • ad9680

    When I connected ad9680 and FPGA, I found the following:
    After powering on, disconnect the ad9680 sampling clock, and then connect it again. It is found that 1.ad9680 and FPGA's jesd204 channel is difficult to establish. Only by pressing the reset button…

  • ad9680

    I would like to ask, in the process of establishing the ad9680 link, will the ad9680 sample at this time, or not. If the sampling is still performed, is the data sampled during the link establishment process lost or cached in a certain device, and then…

  • ad9680

    I would like to ask, in the process of establishing the ad9680 link, will the ad9680 sample at this time, or not. If the sampling is still performed, is the data sampled during the link establishment process lost or cached in a certain device, and then…

  • ad9680

    Does the ad9680 start sampling or stop during the link establishment period?

  • ad9680

    Does the ad9680 start sampling or stop during the link establishment period?

  • AD9680

    AD9680, sampling rate fs = 720M, intermediate frequency f0 = 930M, 8 times decimation, how to configure registers such as 0x570 0x200 0x201 0x310 0x330 0x311 0x331?

  • AD9680

    AD9680 中频f0=930MHz,采样率fs=720MHz,做8倍抽取应该如何配置寄存器0x5700x200 0x201 0x310 0x330 0x311 0x331 0x314 0x315