• AD9674 Problems with Trigger

    Hi there,

     

    Unfortunately we need help with the commissioning of the AD9674.

    We program the device via SPI as described in the data sheet. We use the chip grade of 80 MHz and the 12 bit operation without RF decimator and have adapted the places in the…

  • a question of use of ad9674

    Hello,

    I'm bringing up a board with AD9674. I Initialized the chip as suggested in the datasheet. In result I'm getting dclk and fclk out, but the data lines are always '0'. Any suggestions what may be missing from the config? I would expect data lines…

  • AD9674

    AD9674当采样率大于65msps的时候,必须使能抽取器,我想问一下,有没有办法不使能抽取器,使其采样率达到100MSPS

  • AD9674

    Hi

    I want to use ad9674 in ultrasonic ndt product, I am not very happy run at 65MSPS. But seems that if use sample rate higher than 65M, we need to use RF decimator. I know the the lvds output was limited to 1G bps, I want to know if I can run sample…

  • RE: AD9674 init problem

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Decoupling AD9674 on PCB

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD9674与AD9276数据采集

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ad9674 maximum sample rate

    Hi

    I want to use ad9674 in ultrasonic ndt product, I am not very happy run at 65MSPS. But seems that if use sample rate higher than 65M, we need to use RF decimator. I know the the lvds output was limited to 1G bps, I want to know if I can run sample…

  • AD9674 TGC Gain input driver

    Hi,

    For AD9674, we need a differential driver for Gain+-, in datasheet figure38, there is reference design, but this design need an input from -1.6V to 1.6V, except a DAC, we need an OP amplifier to convert to bipolar output. and for this amplifier,…

  • AD9670/9674 - individual channel power-down

    Dear Analog team,

    I would like to have additional information about the individual channel power-down feature on the AD9670 and AD9674 components.

    The datasheets indicate that bit 0 in register 0x022 (SERIAL_CH_STAT) controls channel power-down. Do you…