Hi Dougl,
I've been trying to get the AD9695-1300EBZ eval board to work with the VC707 Virtex-7 FPGA board. Would it be possible for me to get some example code as well? I'd be super grateful!
My email is:
hmahn@g.ucla.edu
Thanks so much!
Hi Dougl,
I've been trying to get the AD9695-1300EBZ eval board to work with the VC707 Virtex-7 FPGA board. Would it be possible for me to get some example code as well? I'd be super grateful!
My email is:
hmahn@g.ucla.edu
Thanks so much!
Hi Jerry.X,
Thanks for your interest in AD9656. I'll request that the sample FPGA code be sent to you.
Doug
Hi ADI Team,
I am using ADC AD9656 in my new design.
I need only two Analog input Channels. Other two Channels are not required.
Shall i left them floating or any termination required?
Thanks,
Sakthi
Hi,
I'm working on ZCU102 with AD9656. can I please have have HDL.
Also Anyone tried with ZCU102 or any recommended board.
Thanks in advance
S
Hi,
I am using the 16bit-AD9656 in an FPGA project. I am able to receive data from the ADC, but would like to validate the 6Gbps link using the PN23 PRBS testmode. My VHDL PRBS-checker has been validated using real ADC-samples in another FPGA project…
I have compared the hardware design to the reference design, there are no differents.
I mearsure the devclk/sysref to ADC and FPGA, the clock is right.
Now I configure AD9656 to ML=42, 100MHz sample clock, line rate = 4Gbps, and I connect 2 AD9656 to the…
I experienced the same problem。Sometimes FPGA can received K28.5 and ILAS, but sometimes FPGA can't, and FPGA transceiver encouter the "8b/10b not in table" errors, and cause the link is down.
And how do you solver the problem?
Hello. I have a question about the programming of the AD9656 and some inconsistencies I see between the SPIController software and the datasheet. We are working on custom PCBs, so I am using SPIController just to produce a script file that I can use to…
I am trying to connect the EVAL-AD9656 to a zcu102 board and I cannot find the FMC pinout and IO standards documented anywhere. Do you know where I can find this information so I can create an .xdc for the fpga?