将一个一个峰峰值为2.7V频率为50MHZ的正弦波给AD9632放大2倍(按照手册上的典型电路接的)想要放大到5.4V可是输出自激,似乎AD9632的输出峰峰值为4V才不会自激,只要比4V大就会自激,AD9631做电压跟随也是同样的问题,只要输出比4V大就会自激。请问这是怎么回事(频率为50MHZ)。求专家解答,比较急,万分感谢!(推荐输出能力比5V大的芯片也可以)
Hello teacher,
I use VIVADO2016.2 to build MICROBLAZE minimum system debugging AD9361, hardware platform is KC705, builted 9361 project with SDK2016.2, when i build project that promat data overflow, I have changed address space of "sys_dlmb_cntlr "…
Hi all,
Is it acceptable to connect the -Vs supply input of the AD9631 to ground (and let's say +Vs = +3.3V)? I would like to remove a -3.3V supply from my board which has an AD9631 on it and just use ground as -Vs. Currently, I have a 200 ohm resistor…
Hi Everyone,
I am using AD9631 for one of our project, my design flow are as follows,
ADC part
1) Driving analog signal from outside through SMA connector.
2) An RF transformer to convert single ended to differential signal.
3) Driving this differential…
analog-admin
Hi everyone,
I am a new user of AD9631, now I want to realize point to point transmission, could you tell me where can i get the sending and recieving program, it will be better if you send these programs to my mail(Wenyang.Xiao@verisilicon…
Hi
I use AD9361 & AD9634, only for transmission.
With both components I encountered the following problem:
Determining tx bandwidth using the appropriate function - does not work.
I work at a transmission baud rate of 2MS, and I want to set bandwidth…
Hi all. I recently have a hard work that is to change Pluto to support 2r2x. I find that Pluto uses the AD9631 FPGA core which supports 2r2x,and the pluto hardware schema already has 2r2x ability ,but Pluto just use 1r1x, so from the hardware point of…
Could anyone give an example to set the FORMAT_SIGNEXT bit in the REG_CHAN_CNTRL register using the direct_reg_access? should I use ad9631-phy or cf-ad9631-lpc? Thanks. Is the following correct?
>cd /sys/kernel/debug/iio/iio\:device4 # device4 is the…
Hi
I use AD9361.
I also encountered this problem.
We work at a transmission rate of 2MS,
but no matter how much I increase the BW (I checked up to 20M)
I get a bandwidth of 2M,
I also use AD9634
We encountered the same problem, where we were able to solve…