Hello, I want to build a simple VNA (vector network analyser) and I am interesting in buying the AD9631 chip.
I would like to know if it is possible to control the AD9631 chip with a microcontroller using C programming language??
I have seen the suggested…
山东青岛,关注运放AD9631
Hi Supporter,
what is the output range of DAC on AD9631? is it programmable? where can I find the detailed information of the DAC and Mixer modules?
Thx
Hi all,
Is it acceptable to connect the -Vs supply input of the AD9631 to ground (and let's say +Vs = +3.3V)? I would like to remove a -3.3V supply from my board which has an AD9631 on it and just use ground as -Vs. Currently, I have a 200 ohm resistor…
Please don't open multiple threads regarding the same issue. The discussion will be continued here: ad9631 projects "no source avaiable for "_start()"
Thanks,
Dragos
Hallo Andrei,
I have some questions regarding the streaming of sine waves via Simulink.
1) The example of the AD9631 streams two sine wave to the target. Can I do same with the AD9739a and is it possible to stream user defined Signals over this path…
I have do some test on the AD9631 demo board ,we can get the right data from rx port .but on ourself board , we always get the wrong data like constellation rotates.
I have a different filter profile than what is supplied in the AD9631 Eval software. How do I go about getting new coefficients from ADI?