• RE: AD9600 input impedance

    Hello,

    The AD9600 is the 10-bit version of the AD9627.  Link to S-parameter for the AD9627 (and AD9600)  is below.  You can use this S-parameter model along with transformer +R-L-C components when designing an input network for the AD9600 (see app note AN827…

  • ADC driver circuit

    Hi,

    I have a board where an AD8138 Differential Driver is driving an AD9627 ADC.

    The circuit is exactly the same as the one shown in Figure 46, page 27, of the AD9627 Datasheet.

    In the AD8138 Datasheet, page 3, it is indicated that the Offset Voltage…

  • RE: problem with FPGA board

    Hi,

    If I am interpreting your post properly, you have the AD9627 + EVALC working, but you need to trigger the data capture to synchronize with another event.  Is that correct?  If so I can see if we could possibly support that.  Can you tell me any more…

  • 关于AD9640差分时钟、模拟输入与PCB布局的使用疑问

    最近在使用AD9640进行硬件设计

    差分时钟部分:

    疑问1:datasheet在差分时钟部分提供的参数芯片是95xx系列,这些芯片是不是对输入的时钟信号质量要求也很高?在时钟次系列芯片的时候需要注意哪些事项?次部分的参考地是否需进行与模拟/数字地进行一定的隔离处理?

    疑问2:如果外部没有高精度的时钟源设备,是否有替代方案可以实现单端转差分时钟输出?并且时钟抖动质量可以在100fs-300fs之间?

    疑问3:是不是使用PLL类型的时钟发生器芯片带来的抖动误差会比较大?针对14位的ADC输入差分时钟有此类型的参考吗…

  • 关于阅读<模数转换器时钟优化:测试工程观点>文档时的疑问

    <模数转换器时钟优化:测试工程观点>

    (1)P.1中提到的公式1与2的疑问

    为何文中提到“使用具有350fs抖动的时钟测试14bit ADC,为了避免性能下降,输入信号频率必须低于35MHz”,这里的35MHz是怎么计算得到的?

    按照公式2得到的SNR=6.02*14+1.76=86.04;然后按照公式1反推输入频率f得到的是22.685MHz,这里的计算还有那些需要考虑的吗?

    (2)在AD9627的P.30中提到输入时钟有一个DCS功能,这个在实际应用中,我应该如何评估外部时钟的jitter最差可以到多少可以满足性能不会变坏太差呢…

  • problem with the evaluation board

    Good day! Our group works at the JINR (Joint Institute for Nuclear Research, Russia, Dubna) and we engage in automation and data processing in physical experiments. We bought an Analog Devices HSC-ADC-EVALC board last year. Our aim is to digitize signals…

  • 参与问题讨论,赢智能红外遥控wifi开关

    首先,本期活动至针对本群组成员哦~

    回复以下亟待征求的问题,有机会获得【天猫精灵定制 博联智能红外遥控wifi开关】

    (根据参与的问题次数以及质量选取获得者)

    AD9627的SPI无法写数据,只能读数据。

    AD9833输出正弦波偏置问题

    AD7792在批量使用中出现损坏

    AD9789 issue for DTMB

    关于AD7177-2如何进行双极性单端电压采集

    AD7172读取ID寄存器后不能正确读取数据

    AD7190采样原始数据不稳定

    ADG3247电平转换