• Issues with AD9627-150EBZ

    I have some issues with your ADC evaluation board AD9627-150EBZ (https://www.digikey.es/product-detail/es/analog-devices-inc/AD9627-150EBZ/AD9627-150EBZ-ND/1762652).

    Namely, I am driving the board with the following signals (please find the pictures attached…

  • AD9627, output data port layout routing

    Hi,

    I am trying to create the layout for AD9627. I am confused with routing AD9627 output data port.

    Since this is high speed ADC the data port should also be high speed and should be able to support high speed communication. My question here do we…

  • AD9627是怎么采样的?

    现在使用的是AD9627+FPGA(AX3750),使用一个接收例程来接收信号,只配置了2 个寄存器的值,一个是寄存器0x14,另一个是寄存器0x FF。对寄存器0x14配置成LVDS输出格式,输出为offset binary模式。对0xFF寄存器的最低位写1生效,请问AD9627是对信号怎么采样的,有IQ采样吗?

  • AD9627是怎么采样的?

    现在使用的是AD9627+FPGA(AX3750),使用一个接收例程来接收信号,只配置了2 个寄存器的值,一个是寄存器0x14,另一个是寄存器0x FF。对寄存器0x14配置成LVDS输出格式,输出为offset binary模式。对0xFF寄存器的最低位写1生效。然后想问问AD9627是对信号怎么采样的,有IQ采样吗?

  • 关于AD9627在使用上的一些疑问

    AD9627使用的问题:只使用一个通道是否也可行?

    看手册的P43页关于0x05的说明,可以只选择一个通道作为输入?

    如果是这样的情况,是不是另外一路的供电还是处于工作模式?只是没数据输出吗?

    因为看电源模式寄存器0x08所列的只是全局性的模式设置,并不能指定某个通道进行关闭吧?

    这样会对使用的ADC性能造成影响吗?

    另外的问题是:

    (1)ADC的性能的好坏是不是主要集中在:低抖动的输入时钟,稳定的基准参考?

    (2)数据输出的缓冲级使用74avc244或者74avc245,孰优孰劣呢…

  • AD9627的SPI无法写数据,只能读数据。

    你好 ,ADI专家。

    有个问题求助一下,最近在用AD9627,但是它的SPI模式始终无法写入寄存器数据,但是SPI可以正确读出相关寄存器的默认值。 SPI接口是用FPGA来做的。也是就是AD9627只能读出寄存器数据,无法写入寄存器。

    而且用示波器测量了SPI的三根信号线,时序是满足datasheet要求的。

    不知道这是什么原因?

  • 关于AD9785-DPG2-EBZ和AD9627-150EBZ 这两款评估板

    您好!我买的AD9785-DPG2-EBZ和AD9627-150EBZ 这两款评估板是否可以通过背板连接线连在一起实验。即将模拟信号经过我的这个AD评估板,然后直接经过DA评估板,转换为原来的模拟信号?这个方案可行吗?如果可以的话,应该怎么连接这两个板子的连接器件将这两个板子连接在一起了?如果不可以的话,原因是什么了?

    另外一个问题:对于AD9627这款评估板(绿色的),背板连接器的输出信号是哪些引脚了?同样,对于AD9785这款评估板(蓝色的),背板连接器哪些引脚是输入信号?也就是这两块板子的背板连接器该如何连接起来了…

  • AD9627 数字中频信号驱动能力问题咨询

    准备设计一块单板,ADC型号为AD9627,数字中频信号接口配置为 1.8V CMOS, 通过FMC 连接器和Xilinx VC707 FPGA开发板互连,FPGA 开发板FMC 连接器到FPGA芯片走线长度约9000mil。查看AD9627芯片手册,片类自带一级Buffer,不知道AD9627数字IO是否可以直接连接到FMC 连接器?如果直连信号质量是否有保证?还是需要外部再加一级Buffer?谢谢!

  • when input clock is 125MHz, ad9627-125 works well, but not work well when clock is 100MHz

    Hello,

    we have some problems

    when input clock is 125MHz, ad9627-125 works well, but not work well when clock is 100MHz, why?

    thank you!

  • RE: AD9600 input impedance

    Hello,

    The AD9600 is the 10-bit version of the AD9627.  Link to S-parameter for the AD9627 (and AD9600)  is below.  You can use this S-parameter model along with transformer +R-L-C components when designing an input network for the AD9600 (see app note AN827…