• ad9576 Symbols & Footprints

    Hello 

    On  the ADI web  site  there is no  information about  symbol and  footprint  for Ultra Librarian. 

  • AD9576 X103Default value

    Table 41 shows 0x103 default value is 0xE8

    But tabel 47 shows 0XE0(Bit4 is not same)

    which value is correct?

  • RE: AD9576 PPRX PIN SETTING

    No. With SP0=SP1=1 all register programming is via the SPI pins (CS, SCLK and SDIO).

    The PPRx pins allow you to automatically select predetermined device configurations by connecting resistors of certain values from GND or VDD to the PPRx pins. The PPRx…

  • AD9576  INPUT ONLY REF0

    1) Input of AD9576 will use only REF0. 

       in that case, REF2 and PLL1 aren't used ,Isn't an oscillator for REF2 necessary?

    2)When not loading an oscillator for REF2,

       I understand that Reference Monitor can't move. Are there other functions which…

  • AD9576 SDIO OUTPUT Current

    Dear supporters,

    Please tell me the drive electric current ability of the SDIO terminal.

    (I'd like to connect to MCU of 1.8V, so please tell me because I'd like to insert level shift circuit at time.)

  • 2个或者多个ad9576如何同步能使其输出时钟相位同步对齐?

    大家好

          2个ad9576怎么才能芯片之间同步输出的时钟相位,现在我的系统需要用2个ad9576来驱动16个ad9265,每通道采样100MHz,16个通道之间需要采样时钟相位同步,一个ad9576的0-8输出时钟驱动8个ad9265。请问2个ad9576之间怎么实现同步相位?

  • 2个AD9576之间怎么实现同步来保证16个AD输出时钟相位都同步?

    我的系统现在需要用2个AD9576来驱动16个AD9265 100MHz/ch 采样,每片AD9576驱动8个100MHz的AD采样时钟,16个AD采样时钟之间需要实现相位同步,1个AD9576的0-8输出时钟之间可以实现相位同步,那2个AD9576之间怎么实现同步来保证16个AD输出时钟相位都同步?

  • Can I produce simultaneous multiple frequencies for CMOS output on the AD9576 EVAL Board?

    My requirements are at least 3 simultaneous CMOS clock outputs of various frequencies across the range from 25 MHz up to 500 MHz and beyond. After reading the EVAL User Guide it is not clear whether this board is able to produce at least 3 CMOS outputs…

  • Can I flash a persistent configuration to the AD9576-PCBZ Eval board?

    The AD9576-PCBZ eval board appears to have an EEPROM built in. Can I flash a persistent configuration to the AD9576-PCBZ Eval board?  I would like outputs 8, 9, and 10 to always power up at 156 MHz without needing ACE to reprogram it. Is that possible?

  • What are the specifications and estimation method for the output frequency accuracy of the clock generator?

    Hi all,

    What are the specifications and estimation method for the output frequency accuracy of the clock generator?

    Our customers are comparing the following two clock generators as candidate devices for new development projects.
    AD9576, AD9577

    We could…