• AD9231, AD9573

    Hello,

    I'm looking for a clock wich I can use for the AD9231. It needs to be a low power device for my design. Is the AD9573 suitable for that? I'll only need the 100MHz output of the AD9573. To wich level do I have to connect the VDD33, 33M and GND33…

  • 关于时钟芯片AD9573和DDS芯片AD9102

    请问AD9102直接数字频率合成器的时钟可以由AD9573产生吗?

  • RE: How to connect hdmi video signal to pci express bus

    Hi,
      Do you have one of our Evaluation board?
      AD9573 is a Clock Generator IC optimized for PCI-e applications.Please refer this http://www.analog.com/media/en/technical-documentation/data-sheets/AD9573.pdf
          Did you refer this thread?
      PCI Express Generation…

  • about AD9102 clock

    Can AD9102 use AD9573 as its clock generater?

  • PCI Express Generation 2 (3)

    Hi,

    the AD9573 is a Clock Generator IC optimized for PCI-e applications.

    This is true for GEN1 (2.5GTs). Is this IC also suitable for GEN2 (5GTs / 6.25GTs) and GEN3 (8GTs)?

    I think, it is, because Bus frequency is still 100MHz?

     

    regards

    Thomas

  • How to Provide RefCLK for AD's DDS chip evaluation boards

    Hello,

    I am looking to use an AD product to create several synchronized sinusoidal signals with excellent phase resolution.  I would like to purchase evaluation boards for one of the following products AD9854, AD9959, AD9914 but have not decided which…

  • TAGS LIST: Clock and Timing

    LTC6953
    LTC6955
    LTC6957-1
    HMC6832
    HMC7043
    LTC6950
    LTC6954
    HMC987
    AD9576
    AD9508
    HMC1035
    HMC988
    HMC1033
    HMC1034
    HMC1032
    HMC1031
    ADN4670
    ADCLK944
    ADCLK950
    ADCLK948
    ADCLK846
    ADCLK954
    ADCLK946
    ADCLK854
    AD…