• Ad9550 10mhz frequency multiplier to 40Mhz reference circuit and configuration circuit

    Ad9550 10mhz frequency multiplier to 40Mhz reference circuit and configuration circuit

    If the AD9550 can't be realized, I recommend another chip, you can enter the AD9269

    THANK YOU

  • ad9550 10mhz倍频到40Mhz的参考电路与配置电路

    ad9550 10mhz倍频到40Mhz的参考电路与配置电路

  • RE: AD9550 PLL Lock Failure

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: 寻求一款10M倍频到40M的芯片,配套AD9649

    您好,感谢对ADI产品的关注。

    您可以看一下AD9550,是较新的双通道时钟产品。

    https://www.analog.com/media/en/technical-documentation/data-sheets/AD9550.pdf

  • RE: AD9265 cmos clock driver

    Do you suggest me any other low jitter clock generator which can generate 42.8MHz clock from 50Mhz clock oscillator ?

    what about AD9550 ? can it generate 42.8MHz from 50 MHz oscillator ?

  • LVDS and LVCMOS output clock in phase

    Hello all

    I was looking for a "simple" PLL that can generate two clocks, a fast one (eg: 480MHz) and a slow one (eg: 48 MHz) with a known and fixed phase between each other. Ideally the phase is 0. But in any case, I can't find very accurate phase relation…

  • RE: 低抖动时钟合成器

    看一下AD9550 AD9552/53是否满足你的要求

  • RE: Alternate crystal frequency for AD9575

    Hello Alex,

    The key parameter here is the VCO frequency, which is rated at 2488 to 2550 MHz over process, temp, and voltage (PVT).

    Unfortunately, 135 MHz would require either a 2430 or 2565 MHz VCO frequency that is outside the allowable range. Now…

  • TAGS LIST: Clock and Timing

    LTC6953
    LTC6955
    LTC6957-1
    HMC6832
    HMC7043
    LTC6950
    LTC6954
    HMC987
    AD9576
    AD9508
    HMC1035
    HMC988
    HMC1033
    HMC1034
    HMC1032
    HMC1031
    ADN4670
    ADCLK944
    ADCLK950
    ADCLK948
    ADCLK846
    ADCLK954
    ADCLK946
    ADCLK854
    AD…