Dear Specialist,
Sorry to trouble, can you help to check whether we can directly read out the TDC and NCO value of AD9543, i can only find auxiliary TDCs' read register.
Hi,
Can I get source code of AD9680 and AD9543 drivers compatible for linux kernel version 4.14
Thanks
I have a design using the AD9543, that currently uses only two channels connected to a DDS and an ADC. The Ref clock is not used (but in the design) and the clock input is a 25Mhz TXCO
The M outputs are set to show that the system clock PLL, APLL0…
HI,
the script uses the cso file created by ACE using the right plugin (that is if you want to configure AD9544, you use the AD9544 plugin to create the cso file). The eventual default values are included in the cso file.
So the script can be used by…
Hi Charly,
I would like to obtain a clock rate as close as possible to 100MHz while still using the 122.88MHz clock. This could be approached with values such as 4*(B=55)+(A=0)=220, and then letting the clock divider be set to 180. How do I change AD9543…
I'm sorry to say, but there is no simulation tool for the AD9544. Please use the AD9545 rev B data sheet as reference for the AD9544 because the AD9544 data sheet has not yet been updated to the detail level of the AD9545. Both chips are from the…
first I want to point out that the AD9542 and the AD9544 do not have auxiliary NCOs and auxiliary TDCs. The AD9543 and AD9545 have them.
The source profiles refer to the DPLL sources. Please do not confound them with the DPLL translation profiles…