Hi ADIer,
I am playing with AD9540EVM, but the LVCO-4505 is obsoleted, I can not find the D/S.
What is the frequency range of this VCO?
Thanks!
J.C.
Hello all,
I have a clock generator AD9540 DDS Evaluation Board, I am using the Eval Software to control and specify the clock to generate. I need a solution to control my DDS Clock with Matlab if possible.
Thank you
Best regards
Said FARAH
Hello
I have an error when installed the AD9540 evaluation software Rev. 1.0.0 in windws XP with the driver of the Evaluation board instaled also. After executing the software, the message 'Runtime error '13' "Appeared in windows.
…I have installed the AD9540 evaluation software and drivers on a 32-bit Windows XP system and can't seem to get a response from the output of the board. This board has an onboard VCO clock, from which I also cannot measure a response (J16). I have…
Hi Experts,
Follow snapshot is the pll lock status from AD9540, is it an analog pll lock signal. I am wondering if the PLL is in normal locked status.
Regards,
Jason
Accubeat, one of my customers, is looking for CLK distributer with CML outputs, and following requirements:
Nubmer of Inputs: 1
Number of outputs: 4
low jitter and low skew performance.
The output clock frequency range: 1Hz - 2GHz
I saw a AD9540…