• AD9518-1 Pinout

    The OrCAD Capture CIS symbol created by UltraLibrarian from AD9518-1ABCPZ.bxl has the inverting and non-inverting pins of output channels 0, 1, 2, and 3 opposite from what is show in the AD9518-1 datasheet. Can it be assumed that the datasheet is correct…

  • AD9518-1 no output

    Hello,

    we design a system with ad9518-1, but AD9518-1 pin outputs DC 1.6V, and the complement pin output DC 2.4V,  no clock output, why?

    Thank you!

  • AD9518-1 - Script with registers settings

    Dear supported

    My customer is using the AD9518-1.

     

    Required Fout= 122.88Mhz on out4 (780mv) . The external Reference clk on REF1 is 25Mhz.

     

    Currently it seems like the PLL is not working,

     

    1. 1.      We get ~1.2Ghz from VCO + clocks on output0…
  • AD9518-1 eval board unlock/horrible phase noise

    I just received the eval board for the 9518-1 and it has very bad phase noise performance. 1st off I have tried to lock it to a 10,20,50,100 or 200 MHz clock in both single ended, on ref1 or ref 2 and as a diff signal on both inputs. I am trying to generate…

  • AD9518 Sync

    I Have two Ad9518's in different slots of my system that have the same 10mhz input clock in common. Both AD9518's are also configured to generate a 400Mhz clock on output 0&1. I'm trying to figure out how to phase align the outputs and I figured that…

  • AD9518 Calibration

    Hello,

    I’m using an AD9518-0 on my electronics board and now I’m facing some trouble to get the card “ready to serve” after an electrical reboot. In the FPGA connected to the AD9518-o(via SPI), I’m programming all the required settings right after the…

  • 问题: AD9518内部锁相问题

    版主好:
    现在使用AD9518-1,REF1输入频率为40M,R
    divider设置为8,A=0,B=15,P=32
    想用内部锁相环和VCO输出2.4G,内部锁相环已经设置为on。VCO也已经可以校准。
    读取0x01F的值为0x4E,锁相环未锁定,请指教!
    寄存器设置如下
    AD9518_WDATA(0x00,0x00,0x18);

    AD9518_WDATA(0x00,0x10,0x7c); //PLL enable
    AD9518_WDATA(0x00,0x11,0x08);
    //01 R=8
    AD9518_WDATA…

  • [EVAL] AD9518-3A/PCBZ board size

    Hello,

    Do you have AD9518-3A/PCBZ board size information?

    It is listed as EVAL product for AD9518-3.

    Thank you for your help as always.

    Best regards,

    Sofy

  • RE: AD9518 output signal can not be locked, and I need want get help.

    hi,Thank you.

    I have modified loop bandwidth 75KHz for AD9518-1 and output signal can be locked.using ADISimclk ,loop bandwidth 50Khz for AD9518-0 ,its output signal can be locked,also .

  • AD9548 v AD9518, comparison of phase noise performance

    I would like to know if the AD9548 would improve the phase noise performance in
    comparison with the AD9518 for my application?

     

    The AD9548 (if driven with an 50 MHz crystal on the system clock) may or may
    not have better phase noise…