Hi seniors.
I'm trying to evaluate AD9517-4 using EVAL-AD9517-4 board and facing to a trouble.
At first, I tried to use example setting which put on ADI Web site; AD9517_4_EvalBoardExample_In20MHz_Out200MHz.stp.
# The file can be gotten from http…
我选用的是AD9517-4来驱动AD9257,AD9257的参考输入是单端的,直流耦合10MHz,想产生40MHz采样时钟,但是配置完后,把寄存器值读出来了,跟写进去的一样,但PLL没有锁住,那个LD默认检测的是digital lock detect,用chipscope抓取的这个引脚信号是周期性脉冲,意思是锁住一下,又没锁住,不知道是什么原因,还有大家说的AD951X寄存器产生软件,我没有找到。只下到一个SImCLK那个软件
Hi engineer :
I want to use HSC-ADC-EVALCZ to configure my AD9517-4 circuit.The scheme as follows.
The Interface is same as AD9484-500EBZ. Then I loaded AD9517_for_AD9268EVB.cfg and AD9517_for_AD9268EVB.cal file through SPI Controller.The files as follows…
I have AD9484-500EBZ and HSC-ADC-EVALCZ development board.I want to use HSC-ADC-EVALCZ to cofigure AD9517-4.Can you provide example codes to us.I see the scheme is use CY7C68013A to configure AD9517-4.Thank you very much.
Hello!
We are using AD9517-4 for reference frequency set generation: 400MHz, 200MHz and 100MHz. We used GXO-E72 100MHz PECL crystal oscillator as reference.Our problem is - there is too much noise at offsets between 100Hz and 100kHz.
Reference (100MHz…
My design is based on the reference design: UG-328-DesignSupport from Analog Devices, Basically it consist of a AD9517-4, and the AD9253. In my design I program the different blocks from a Zynq FPGA.
I am trying to program the AD9517-4 with no completelly…
Dear Sir,
we are trying to programm AD9517-4 via 4-four wire SPI. Prior to SPI data flow we set PD (power down) pin to low. Then we send
1. Write 0x99 to SPI Configuration Register to select 4-wire interface
MOSI: 0x00 0x00 0x99
2. Write Update…
I have started using AD9517-4. Could anyone give me any advice as below?
On page4 in datasheet Rev.E, there is information about REFIN. I use only REF1 and I put 0.1uF at REF2.
So I use this device as single ended mode. I put 10MHz via 0.1uF DC cut…
各位专家好:
我使用AD9517-4时钟芯片产生LVDS差分时钟以供AD9653使用,现在AD9517-4使用外部采样时钟80M,通过使用AD9517软件得到AD9517寄存器的配置表,利用单片机430_5324的SPI配置AD9517,配置不成功,有几点困惑:
1、关于VCO标定,我的设计不使用VCO,是否还需要对VCO进行标定,是否必须通过参考时钟标定;
2、AD9517每个寄存器之间的配置是否需要延时,是否可以一次把所有寄存器的值写进buffer,最后update寄存器;
3、关于AD9517…