• RE: About BAPASS pin of AD9516-3

    HI,

    I took an AD9516-3 eval board and I plugged it in. I measured BYPASS pin as a continuous voltage at 2.5V.

    Then I created a configuration controlling a clock at REF1 pin. The PLL locked and created an output clock. I continued to measure 2.5V at BYPASS…

  • AD9516-3 Thermal resistance

    Hi, My Job is Thermal Engineer. Flotherm user

    AD9516-3 Thermal Datasheet :  Theta JA (24℃/W)

    I want to Theta JC and Theta JB (4-layer board in still air in accordance with EIA/JESD51-7)

  • 关于 AD9516-3内部VCO工作频率的问题

    您好,

    我使用外部10 MHz的晶振给AD9516-3提供参考时钟信号(REF引脚为single模式),使用AD9516-3内部VCO和PLL来产生时钟信号,调节P、A、B、R来设定VCO频率。

    调试过程中我发现,VCO工作频率在2050 MHz以下时,PLL是可以锁定的,超过2050 MHz就无法锁定(调试过程中,各单元的频率范围都满足数据手册要求)

    但是数据手册显示:内部VCO的工作频率是1.75 GHz-2.25 GHz。

    那么为什么实测中内部VCO工作频率不能达到2.25 GHz呢…

  • AD9516-3时钟芯片配置

    特性:

    VCO频率范围:1750Mhz~2250Mhz6LVPECL(最大输出频率1.6Ghz)输出和4LVDS输出(800Mhz)

    内部结构:

             如下图所示,常用引脚说明:

    REF1:参考输入1

    REF2:参考输入2

    REF_SEL:选择是参考输入1或者参考输入2

    LF:环路滤波器输出,使用内部VCO时使用

    CLK:外部VCO输入

    SYNC:同步输入,低有效,如果不同步,直接拉高。

    REFMON:参考的输出,详细看datasheet

    STATUS:状态输出,详…

  • Unused pin of AD9516-3

    Hello, I have some questions about AD9516-3.

    When using an external VCO, how the LF pin should be ?  Should the LF pin be connected to VS, GND or others ?

    And could you tell me other attention when using an external VCO ?

  • AD9516-3电源电流

    AD9516-3的三类电源VS、VS_LVPECL、VCP的电压都有明确注明,CN0243中电源是同一电源,但现在需要每路单独供应,能否给出每路电源的电流消耗?

  • AD9516-3时钟源咨询

            你好,现在有一款项目我打算使用AD9516-3时钟芯片,考虑到时钟源的稳定性,直接决定了AD9516-3的时钟输出,我的时钟源输入是10M,希望ADI工程师可以给我推荐一款,相位噪声和稳定性都比较高的产品。

          PS:1 依据ADIsimCLK,推荐的是TCX010或者一系列,但是现有资源我无法从网上获取,如有请提供,没有请给我推荐一款。见图。

                  2  附录是我选择的时钟源,请问是否符合要求,请点评!因为这个是OCXO,TXC技术支持提示并不是所有的时钟芯片都支持OCXO的输入。谢谢!

  • should i need to configure AD9516-3 every tiem?

    Hello everyone,

    I am prepare to use this chips-AD9516-3 in my design. So i'm full of curiosity about how to configure this chip. Does it has the ability to remember the value of Regs which have been written. I need to configure this chip after power…

  • AD9516-3开发板USB识别问题

    工程师你好

    我们实验室近期购买了AD9516-3的开发板调试用,发现电脑无法识别USB驱动,如下图:

     

    该板卡采用Cypress公司的CY7C68013A-56PVXC芯片作为USB驱动芯片,我们从其官网下载并安装了CySuiteUSB3.47程序包,但是其USB无法识别问题依旧无法解决

    我们电脑的系统是WIN7 32位,按照AD公司和Cypress公司的相关文档说明是没有问题的,您能帮我解决下该问题么?

  • how to connect REF_SEL of AD9516-3 when the REFIN is differential pair?

    hello,

    Recently I make the AD9516-3 to output 1G ,250M and 200M from the REF_SEL 200MHz. I plan to connect the REF_SEL of AD9516-3 to 200M difference clock from external chip.but How do I connect the REF_SEL? The datasheet only tells me about REF_SEL…