Dear friends, I have a problem in programming AD9516-3.I have programmed the register map for the following configuration.
VCO is locked correctly but I don't have any outputs on OUT0 ~ OUT9!any comment is welcome.
Thank you
1. May I ask whether the sma interface of CLK on ad9516 evaluation board can only be used to access the output of external VCO?
2. I want to connect a 150MHZ clock to the ad9516 evaluation board, but it reminds me that it is beyond the scope of the PFD…
I have two ad9516 evaluation boards, one is ad9516-1, the other is ad9516-5. When I used it, I found that the LD light on the ad9516-1 evaluation board could be normally lit after downloading the same program, but the LD light on ad9516-5 couldn't be…
Dear All,
I am using the AD9516-0 to clock the AD9122.
Around the 983.04MHz, I can observe a lot of spurs every 61.44MHz.
What is the maximum reference spurious…
Hi,
You can use 'spi controller' to access the AD9516 control.
The DAC Software Suite is included on the Evaluation Board CD, or can be downloaded from the DPG web site at https://wiki.analog.com/resources/eval/dpg/dacsoftwaresuite. This will…
Hello
R = 1, PD = 8, A = 0, B = 3
The loop filter is the same schematic with AD9789EV.
Ref in-100MHz , OutCLK-2.4GHz
PLL Frequency locking is well.
Phase noise is fine.
But the frequency of 1~10KHz offset the shakes.
What is the problem?
check…
Hi, My Job is Thermal Engineer. Flotherm user
AD9516-3 Thermal Datasheet : Theta JA (24℃/W)
I want to Theta JC and Theta JB (4-layer board in still air in accordance with EIA/JESD51-7)
I have a rubidium clock, the output common mode voltage is about 0V, I want to use the output of this rubidium clock to send to the CLK interface of ad9516-1, can I input it directly? Or what conversion measures I need to go through.
I have generated the required clocks using two different configurations of the AD9516-1. One mode uses VCO, divides by 2, and thus I need a higher input clock frequency. The other mode bypasses VCO, and thus I can use a lower input clock frequency.
Is…
1.I have an ad9516-1 evaluation board. I want to use two cmos interfaces with different frequencies, but the sixth and seventh interfaces on the evaluation board are not soldered. Therefore, I want to solder the sixth and seventh interfaces, but I don…