• Clock multiplication with AD9516-0/PCBZ

    Hi All:

    I have an AD9516-0/PCBZ. Can I use it to multiply my clock signal from 1 MHz to somewhere between 50 MHz and 120 MHz? If yes, how?

    Thanks!

  • AD9516-0 软件导入问题

    你好,关于AD9516-0软件导入评估板的问题:

    1.在软件中设置好参数后,怎么将参数导入到AD9516-0评估板中呢?

    2.导入后,是否是永久保存的?   我在使用时,发现断电后重开电源,评估板中的软件参数设置就恢复原始了,不是我保存的设置了。这应该如何解决呢?

    谢谢。

  • can EVAL-AD9516-0 keeps the register setup?

    Hi,

    I want to use EVAL-AD9516-0 as clock source for AD9208. 

    I know that EVAL-AD9516-0 has convenient software.

    I wonder if the settings are stored when I set up the settings using the software.

    So, I wonder if EVAL-AD9516-0 keeps the settings even…

  • RE: Mechanical drawing of AD9516-0BCPZ

    HI,

    the AD9516-0 evaluation board page has the Gerber files of the board. These files contains the information you are searching

    https://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-AD9516-0.html#eb-ov…

  • Please tell me the power start-up conditions required by AD9516-0.

    My customers are using AD9516-0, and my customers are facing trouble.
    Customers surveyed about their products and concluded that power supply and POR are suspicious.
    Their products have a power supply that rises slowly.
    The supply voltage rises to 2.9 V…

  • AD9516

    We have used AD9516 clock generator in one of our projects. I made configurations with ADIsimCLK.
    How can I save register configurations to file for later SW writing by MCU?

  • RE: AD9516-0 with passive loop filter and external VCO

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD9516系列芯片该配合什么软件去测试

    您好,感谢对ADI产品的关注。

    ADISIMCLK可以直观的让您看到AD9516的仿真结果。如果您要看实际电路,您可以购买AD9516的评估板配合评估板软件进行实际测试。也可以参考评估板原理图自己设计。www.analog.com/.../EVAL-AD9516-0.html

  • RE: AD9516

    您这个情况应该还是没有锁定。您可以通过回读寄存器0x01F查看lock detect是否正确。很可能还是1M的参考压摆率不够导致。

  • RE: AD9516-0时钟芯片输出时钟频率有偏差

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,