Mcee,
Apologies for the delay. It appears that unfortunately for us the device we've been using to generate our clock frequency is not reaching the Slew rate requirements at low frequencies. So that would be the problem right there.
It also appears…
Mcee,
Apologies for the delay. It appears that unfortunately for us the device we've been using to generate our clock frequency is not reaching the Slew rate requirements at low frequencies. So that would be the problem right there.
It also appears…
I feed AD9514 CLK input from AD9517 output. SYNCB pin of AD9514 is tied with CSB pin of AD9517. After AD9517 callibration finish I read state of AD9517 register once more to synchronize AD9514 outputs, but result is sporadic. What may be a reason of this…
Hi Larry,
We realized the AD9102 evaluation board has AD9514 chip already
installed. We ordered a AD9514 Board. Does the Board buy us something we do
not already have on the AD9102 evaluation board? Our group is up in arms
about that - please comment…
Hello, I want to 40khz sine wave using AD9102/AD9514.
(I have a AD9102 EVM Board It worked well.)
I have some problem using AD9514 Clock divider.
(I choose clock source 180Mhz crystal(XLL336180.000000I).)
1. AD9514 OUT0(LVPECL) just DC Offset…
Hello
I would like to ask i am considering working with one of the components AD9520-4/ AD9514/5
for DDS Clocking and, and i see alot of applications use the AD9520-4 for this purpose, but this component has a lot
of Registers for the pupose i need…
Hello AD community,
I'm looking for help in configuring the outputs of the AD9514 clock distribution chip.
In my project, I anticipate needing only one output, so I have OUT0 configured like I need it. However, I would like to keep my options open…
I agree that you scope can't get the 1milli-degree resolution, but it should be sufficient for the 1.4 degree problem that you are trying to figure out. Currently you don't know if it is from AD9102 or AD7760 or AD9514 or the oscillator. If the scope…