• AD9513: figure 25 full scale delay datasheet error

    In datasheet, it full scale delay should be 1.8ns,6.0ns,11.6ns, programmable.
    But, there is fig. 25 shows the delay is 1.5/5.0/10ns.
    Which one is correct?

     

    The spec table is correct. The spec table undergoes a detailed design review
    prior to…

  • AD9513 freq divide configuration


    Hi. I am in the design of a pcb that uses the AD9513 as a freq divider.
    For my application I need just one output for a freq divide by 10.

    I made a configuration table according to the datasheet.
    If I check the datasheet, table 14 indicates S5 and S6…

  • AD9513 reference clock

    Hi , 

    I am using 2 AD9513 components. 

    I have a clock oscillator of 10MHz , 0-3.3v 3.3vpp.

    The clock reference input of AD9513 requires 1.3vpp AC coupled. 

    So I need to split the 10MHz into two signals of 10MHz.

    And to level shift oscillated signal to 1…

  • AD9513 input level

    Hi,

    I'm using AD9513 in our design.

    In page 17 of the datasheet, it is mentioned " The input level should be between approximately 150 mV p-p to no more than 2 V p-p. Anything greater can result in turning on the protection diodes on the input pins…

  • RE: AD9513

    This question has been closed by the EZ team and is assumed answered.
  • ADSimClk仿真AD9513,

    ADSimClk仿真AD9513时,其中一路输出提供延迟单元,具有3个可选择的满量程延迟值(1.5 ns、5 ns及10 ns),在哪里可以设置啊,还有相位的问题,

  • RE: AD9513

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD9513

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD9513 jitter

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,