Hi,
please send me the schematic of the AD9508 you use and tell me what register or pin configuration you use.
Petre
Hello,
I would like to use the AD9508 with a sine wave input, but it is not clear from the datasheet if this is possible.
Does the AD9508 support such inputs, or do they have to be a square wave?
Thank you in advance,
Yulia
I have a system that uses the Analog Devices AD9508/PCBZ eval board to route clocks to various sinks. It takes a 150 MHz input clock and provides the following:
The output format…
Is the drive current of the AD9508 in HSTL mode 8mA(or 16mA in double amplitude) described in de datasheet(rev E) on page 24 section "Clock Output" or 3.5mA(or 2x3.5mA in double amplitude) described in the register settings on page 35-39…
Dear Analog Devices
I am having challenge in clarifying some details regarding the use of the AD9508.
My intention is to implement the clock fan-out buffer towards three ADV7180 analog video decoders. I suggest to use a 57.2727MHz (+/-25ppm) oscillator…
Hi
I am debugging the function of AD9508. I have configured it in pin programming mode (AD9545 datasheet Pg26), but why the output is 2V level CMOS, which is theoretically 1.8V.
I need 8 single-ended 100MHz clocks and these are have same frequency and phase. I see AD9508 have 8 1.8V CMOS outputs. The problem as follows,
1. I see in the datasheet of AD9508 in page 26 rev .G , look at the red line in the picture below. In "PIN…
Hi All
In the course of reducing the parts count of our Mainboard, I'd like to change the pin strapping resistors for the AD9508 from 820R to 1K. Will the corresponding function be correctly selected anyways? Or is it necessary for the resistors to match…
Analog experts I really need your help. it seems my thesis is going to hell or paradise!
I have concluded a result at the end of this page. is it OK?
according to the AD9508's datasheet:
the output swing is as shown below:
and the output offset…
Hi Analog expert,
Can anyone comment here?
If you dont have idea, then how should we adjust like this matching ?
Thanks Kaos
---
Dear Sir/Madam,
Our customer asked as following question for your AD9508.
He will design the output circuit as following…