• AD9484-500EBZ connect to HSC-ADC-EVALCZ test

    Hello, I bought AD9484-500EBZ and HSC-ADC-EVALCZ. I want to connect them together for testing. But I didn't test the waveform. Where am I doing wrong? The requirements for analog signal and clock signal can give a detailed explanation, thank you. The…
  • AD9484

    Dear support,

    we recently bought an AD9434-FMC-500EBZ board to evaluate on this ADC.

    We also want to evaluate on the pin compatible AD9484 8-bit device,

    but we see that the AD9484 evaluation board is only available for purchase with the non-FMC…

  • RE: HSC-ADC-EVALDZ development board and AD9484 evaluation board

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD9484 common mode

    Hi,

    I went through the AD9484 datasheet, and I was a little bit confused in understanding the input common mode section.

    According to the datasheet, the optimum input common mode is set to about 1.7 V by CML pin. Since the ADC has a 1.5 Vpp maximum…

  • AD9484,Analog input Frequency range?

    Hello,

    I have a question is AD9484,Analog input Freq. range.

    Because Available Input source range is 0.3MHz ~ 60MHz.

    Please send me your comment.

    Thanks and regards,

    Eddy

  • AD9484问题

    根据芯片手册中说明和原理图,当AD9484上电时,vref接20K下拉电阻,但管脚输出为0,且vin+和vin-有一个1.8v(电源电压)的直流偏置,此时vin+和vin-并没有与任何电路相连接.我想问下这个问题该如何解决,spi在设计时选用的都是默认配置.

      谢谢帮助!

  • AD9484, just some questions.

    I intend on using the AD9484 in a multichannel digitizer/processing system.

    8-bits running at 500Msps is great for this purpose.

    I was looking through the datasheet of the chip and the eval board and still had some questions. Even after looking at other…

  • FLEX_VREF  of AD9484

    HI,

         I want use the external voltage reference of AD9484,but the datasheet is confusing ,as it shows,

    BIT 7,6 should be 0 1,use  import Vref, voltage range is 0.59V to 0.8V, but bit 4 to 0 show that Input voltage range is 1.18 to 1.6V, is there any…

  • HSC-ADC-EVALCZ Data Capture Board连接AD9484 Family Evaluation Board 还能再连接一个DA板子吗,HSC-ADC-EVALCZ Data Capture Board上边的Vertex-4具体型号是多少

    HSC-ADC-EVALCZ Data Capture Board这个板子能同时连接DA和AD吗,这样我可以做到通信的收发。HSC-ADC-EVALCZ Data Capture Board上的Vertex-4具体型号是多少,我想看一下他的资源是否能满足我的要求,祝好

  • AD9484 Sample and Hold characteristics

    Hello

    I would like to have more understanding on the sample and hold block at the input of the AD9484.

    Datasheet states that the analog input BW is 1GHz.

    Could you explain what is the sample duration ? how long does the window is opened , and also…