• AD9484 sample question

    Hello,

    I'm using an ultrazed-eg setup with a custom ad9484 board connected. I'm using the ad9467 driver and using ad9517 for the clock. We have it setup and verified our clock is at 500Mhz for 500MS/s. I'm getting some interesting discontinuities in my…

  • AD9484 and  HSC-ADC-EVALC

    Which encoding scheme does the AD9484 use? I would like to determine the time
    it takes to fill the HSC-ADC-EVALC FIFO.

     

    Sample figures on the canvas and DLL execution speed for 64k samples (this is
    the max capture size): 
    The canvas runs at at…

  • AD9484 capture data

    I've used the UG-290 with AD9484 to capture data. But it seems that the voltage is limited between -1V and 1V. How to solve this problem and get the raw data? Thank you!

     

  • UG-290 AD9484

    Hello, 

    I've recently bought the evaluation board UG-290 with AD9484 and HSC-ADC-EVALCZ Data Capture Board. I wonder whether there is an on-board clock to use so that I don't need to connect an external clock. The datasheet has mentioned the on-boa…

  • AD9484 CMRR Specification

    Hello,

    Are there any specifications for the CMRR vs. frequency for the AD9484 500MSps, 8 Bit ADC?

    I could only find the specified CM Input Voltage of 1.7V but no information about the impact of slight variations of this voltage on the digital output…

  • AD9484 input Vcomm query

      Hi ADI Enineers : 

       I  intend to use ADA4939-1 to drive AD9484 , DC coupled , ADA4939-1 output 1V Vp-p volatge , AD9484's CML output 1.7V voltage , so ADA4939's positive output will reach to 2.2V , It seems exceed the absolute maxim VIN+ . Could you help…

  • RE: AD9484外围电路

    This question has been closed by the EZ team and is assumed answered.
  • AD9484输入差分时钟的选择

    对AD9484输入时钟,我选择了一款如下芯片。是否可以直接输入到CLK+端和CLK-端。

    另我如果使用AD9517-4进行配置时钟源,REF输入信号源的要求是什么,有没有推荐的选型?多谢。

  • AD9484-500EBZ connect to Xilinx FPGA board

    We need a 8-bit 500-MSPS ADC to build a mixed-signal system, and the converted data will be processed by a Xilinx FPGA board.

    The evaluation board AD9484-500EBZ satisfies our requirements.

    Can I connect AD9484-500EBZ to my Xilinx FPGA board (FMC connector…