• Interleaving two AD9481 application

    I have two questions about "INTERLEAVING TWO AD9481s ". The datasheet shows the
    description as below figure shown:
    1. The phase offset between two ADCs' Clock should be 180 degree, isn't it?
    2. How we deal with the two ADCs' DS…

  • Strange Behavior of AD9481

    I am designing a laser ranger where the latency of the ADC matters. The ADC is clocked at 250MHz. According to the datasheet, the latency should be 8 clock cycles. Here is the problem: after every the latency changes randomly. Sometimes it is 8 cycles…

  • Hi-Z state of AD9481 outputs

    Do power-down mode (PDWN = AVDD) switches digital outputs of AD9481 to hi-z state? If no, is there any other way to do this w/o external ICs?

  • AD9481 CMOS customer board Rev.A Gerber files

    Where to get Gerber files for AD9481 CMOS customer board Rev.A PCB from the data sheet http://www.analog.com/media/en/technical-documentation/data-sheets/AD9481.pdf  (pp.26-27) ?

  • 关于AD9481的数据转换输出问题

    AD9481芯片在使用过程中,数据同步时钟信号输出正常。在数据输出时钟信号正常的情况下,出现了下面的问题:

    当检测电压超出转换范围内时,输出全是0或全是1,这种情况下数据输出与期望输出相符,正常无问题。

    但是当电压在转换范围内的情况下数据输出引脚出现高阻态,数据输出与期望输出完全不符,不正常。

    这款芯片的控制引脚也不多,排查了一编,也没发现什么异常,请问这样的问题是出在哪里了?

  • 关于AD9481工作在单端输入模式下的接法,望指导。

    之前参考官方数据手册设计用AD8138芯片完成单端转差分进入AD9481,现在想直接接成单端模式,官方数据手册里也没说仔细,只是提了一下,现在我是VIN+输入信号,VIN-悬空,有数据输出,但是数据有扰动,接近200mV。望大家指导一下。

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…