• AD9467

    In ad9467(dut circuitry) evaluation bord schematic pin no. 13,47,46,45,44,43,42,41 are showing  different different pin names compared to datasheet. why it so?

  • AD9467

    Hi all,

    I'm trying to interface AD9467 ADC with Xilinx Zynq Ultrascale plus MPSoC.

    In context to this i have few questions.

    1. What type of clock i need to provide to the ADC? Is it a Sine Wave or a Square Wave? 

    2.  Can we feed clock to the ADC from…

  • AD9467

    I have a new design that will be using the AD9467 and would like clarification  about data I found in the digital specification of the datasheet for the SPI  bus.

    Revision C page 6 of 32 “LOGIC INPUTS(SCLK, CSB, SDIO)” states that Logic 0  Voltage can only…

  • AD9467-FMC-250EBZ

    I have a Xilinx ZC702 evaluation board and wish to investigate using one of
    your high speed >100MSPS 16bit ADCs to analyse an analogue stream from a Laser
    Receiver Diode.  Is the  AD9467-FMC-250EBZ compatible with the ZC702 dev.
    board…
  • AD9467 Exposed Paddle

    The Gerber files for the AD9467 show that solder paste is
    deposited only on the center square of the exposed paddle PCB layout.

     

    This is just a recommendation so that there is uniform solder flow under the
    chip so there aren’t any …
  • AD9467 output delay

    Hi,

    After a few days spent on trying to interface AD9467 to FPGA. I found that there is a difference in AD9467 datasheet revisions.

    Rev.C has SPI register 0x17 (output_delay)

    Rev.D has no information about output delay adjustment.

    Only after trying…

  • AD9467 drift information

    Hello guys

    My name is Fernando, I work for the Brazilian National Synchrotron Light Source.

    We are designing a fast and broadband four channel digitizer for beam diagnostic pourposes for the next Brazilian light source. The AD9467BCPZ-250 is a natural…

  • ad9467 and Linux

    I've been trying to get the ad9467 FMC card working with Linux on the zc706 and seem to have hit a wall.  I took the project files from the bottom of the AD9467 FMC card page (AD9467 Native FMC Card / Xilinx Reference Design [Analog Devices Wiki])…

  • Regarding AD9467

    Hi there,

    We have chosen AD9467 for our project and trying to interface with Zynq Ultrascale+MPSoC, 
    From AD9467 datasheet,it is mentioned that configuration can be done i.e., setting of parameters like input differential voltage,sampling rate,output…
  • AD9467 synchronization

    What is the preferred method to synchronize multiple AD9467s?  My customer needs four channels to simultaneosly sample.  Additionally, is there a roadmap to multi-channel devices with similar analog performance?