• AD9461 DCO problem

    AD9461  DCO outputs are not coming. Clock signals I have checked at the input of the ADC, It is OK. Can you tell me what could be the reason for this. Apart from that When I am seeing the result in Chipscope It shows "00B7" everytime."

  • AD8131 and AD9461

    Hi!

    After a lot of research, i've narowed down my choice of components to an AD8131 to convert my singe ended signal to differential ended, and the AD9461 to perform the high speed conversion.

    Now, i just a have some doubts around the "common mode…

  • AD9461_SPI configuration file

    I am using the EVAL AD9461.when I use the SPI controller software, there is no
    cfg file for AD9461. Do you have the cfg file for AD9461?

     

    The AD9461 is an older device that does not have a serial port for your
    features, so that is why…
  • AD9461_interlacing multi ADC app-2

    I have viewed the application note "Aperture Uncertainty and ADC System
    Performance", and I learned the important effect of the Aperture Uncertainty.
    In AD9461 datasheet, I found there is something different between Aperture
  • DDC Receiver sensitivity

    Hello.

    We are designing DDC receiver (decided to use AD9461) .

    We must provide sensitivity above -120dBm  (10 dB SNR / bandwidth  12kHz). To simplify  the  calculations I  take unmodulated carrier.

    My preliminary calculations are:

    AD9461 SNR = 77 dBF…

  • how do I know if an ADC is suitable for IF sampling, i.e AD9653 or AD9655?

    I have some question on determining the IF sampling capability of ADC's :

    I've checked the ADCs selection table for ADC > 10MSPS

    • some ADC datasheets explicitly mention that the device is suitable for IF sampling, i.e : AD9461, LTC2195, ..…
  • RE: 频率转换功能IC

    您好!

    相关解决方案和产品请见附件内文档。

  • Magnetic Compatible LNA

    Hello,

    I am working on the RF receiving coil of MRI scanner, and a magnetic compatible low noise amplifier is required to work as pre-amplifier inside the magnetic body. The magnetic field could be 1.5T or maybe up to 7T. I noticed that ADI has a document…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…