Thread closed due to inactivity.
Hello
I consider to connect the AD9364, placed on a custom made board with Raspberry Pi 4 in the following way:
1. Raspberry PI SPI interface will be used for communication with AD9364
2. Raspberry PI GPIO pins will be connected to the AD9364 GPIO pins…
For reference, here is my setup:
Here are my Init_Param settings. Note that I've changed the Tx LO to 2.2GHz and am transmitting from TxB (tx_rf_port_input_select…
Hey,
I am just a beginner, I wanted to know how to program your IC-AD9364?
is it done only with evaluation boards/ kits only?
Like I have seen how the SPI interfacing works... but how to give the commands to the IC?
when I searched it was showing to use…
I am using the following system:
I have been monitoring the SPI traffic and trying to match the SPI register accesses to ADI's no-OS firmware…
Can the TX Power Monitor function in the AD9364 be used in one-shot mode? The reference manual describes continuous vs. one shot mode. The linux driver C code defines a bit to enable/disable the one-shot mode. But the documentation says that the enable…
I am using the following setup:
My goal is to transmit data in Dual-port, Half-duplex mode, SDR using CMOS drivers. I am starting by trying to transmit a constant value on ports P1 and P0…
Dears,sir:
My AD9364 configurations are as below:
1. TDD mode (0x013=0x00)
2. To Alert = 1 (0x014=0x1D)
3. txnrx and Enable(level) by pin control. (0x015=08 or 0x0c)
After initial config done, the ENSM enter ALERT state. The reg 0x017=0x15. I set TXNRX…
TX Mon operation (continuous mode):
--------------------------------------------------
Can you confirm that TX Mon operation in continuous mode is as follows:
- TX Mon delay counter starts after ENSM enters TX state (given that level threshold is either…
Hi ,
Just wanted to know if there are any limit on the rate at which i can switch the LO output? Will it harm the device if i change it at every 2msec?
Thank you.