• AD9288: what is the relationship between RIN and REF?

    Firstly,we want to know external reference input range. And we cannot find this
    information on AD9288 datasheet, but we found this info(figure1),



    We think the range of reference voltage in this table is for REFout, not for
    REFin, right?   And…

  • Could AD9288 support 0.5V or 1V ref and can I use single-ended input?

    1. Does AD9288 (8-bit A/D) accept 0.5V or 1.0V reference voltage ?That is,
    REFinA or RefinB = 0.5V or 1.0V ?
    2. Can I simply feed in my single-ended analog signal to AinA (or AinB)and
    ground the corresponding complementary input (i.e. AinA_bar…

  • 关于AD9288数据手册参考电路中W-HOLE的疑问

    大家好,我近期在查看AD9288数据手册时,发现参考电路中有一个W-HOLE的器件,我查阅了一些资料也没有发现这个器件的具体实物形状,请问有人知道这是个什么?提前谢过!

  • Single ended AD9288

    Dear engineers. I need to get the maximum analog bandwidth from AD9288. Which option is more profitable, to use the single ended input from the fast OpAmp or use ad8132, which has an analog bandwidth less then 475 MHz of the ad9288. Do I understand correctly…

  • ADL5511 envelope interface to AD9288

    I'm trying to figure out the smallest way to interface the ADL5511 envelope detect output to the AD9288.  I don't need the full bandwidth of the detector but up to 50 MHz.  I do need the output of the ADL5511 to be DC coupled to the AD9288 though…

  • RE: AD9288 - Common Mode Input Range

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Impedance matching for analog input of AD9288

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD9288 中频采样出现很多杂散

    用AD9288做GPS中频采样,当输入一个中频15MHz -10dBm的电频干扰时,62MHz采样时钟,对62000采样数据做FFT处理,发现幅度谱在干扰频率附近有很多杂散,如何解决? 求大神帮忙!  用AD9218效果一样

  • AD9288 Digital Input Voltage Tolerance

    Hello, I'm confused about the AD9288 datasheet specification for the voltage tolerance of the digital inputs.  Sheet 3 of the datasheet gives a minimum value for LOGIC-1 (2.0v).  However, the datasheet does not specify the maximum value for LOGIC-1…