• AD9287 interface

    Hello,

    I am trying to receive data from AD9287 with xilinx ZCU102 board.

    Adc gives serial lvds output.

    I am using iserdes to receive the data according to xapp524. I cannot get the right data from the xilinx catch.

    Do you have an example to get the right…

  • AD9287 interface (Xilinx Artix7)

    Hello, i am trying to interface an AD9287 to my artix 7 device. Adc gives serial lvds output. I am using iserdes (selectio) module but the problem is i do not know exact starting time of adc output so there is word framing error. İ could not catch the…

  • RE: AD9287 signals after initialization

    Hi Eren,

    I hope your project is going well. Is this question related to capturing AD9287 data with your Artix FPGA? If so, has the sample FPGA code discussed in another EngineerZone thread helped?

    If you still need the AD9287 FCO data, we can work on…

  • AD9287 Dataout frequency not right

    I  have gotten a problem with AD9287ABCPZ-100, as follows,

    According to the Timing diagram of AD9287 ,when my input  clock is 20Mhz, the frequency of dataout should be 80Mhz ,and the bit clock(DCO) should be 80Mhz ,frame clock(FCO) should be 20Mhz .

    But in…

  • RE: AD9287 clock derived from an FPGA - issues ?

    Hi,

    AD9287 stops operating if the clock signal is removed. It should start working again after a clock input is provided. I recommend issuing a soft reset to the AD9287 through SPI after clock is restored if you are experiencing problem with the ADC…

  • Do you have a good idea for connecting AD9287-100EBZ

    Dear Sir/Madam,

    Our customer will use your AD9287-100EBZ and ML695(Xilinx).

    But they cannot connect due to that there is put the difference type connectors.

    So we need the transfer board in there I think.

    eg-1;

    AD-DAC-FMC-ADC

    We cannot use this…

  • Do you have a good idea for connection AD9287-100EBZ?

    Dear Sir/Madam,

    Our customer will use your AD9287-100EBZ and ML695(Xilinx).

    But they cannot connect due to that there is put the difference type connectors.

    So we need the transfer board in there I think.

    eg-1;

    AD-DAC-FMC-ADC

    We cannot use this…

  • AD9287低温采样噪声问题?请帮忙

    hi ADI专家,

    signal chian: analog input-<AFE-<AD8334-<AD9287-100-<Xilinx FPGA.

    Clock input:epson100M crystal oscillator from TI CDCV304 clock buffer.

    1.8V analog and digital power all from TI TPS5430, analog and digital are from one supply…

  • AD9287输出数据bit速率和位时钟对不上问题求助

    我做了一个AD9287的采样,最近在做好之后,发现数据输出速率和随路时钟DCO和FCO对不上,现象表现为,我采样时钟用的是10Mhz,设置全部是默认设置,那么根据手册,一个采样点生成8bit数据,输出的数据速率应该是采样速率的4倍=40Mhz,数据输出速率也就应该等于DCO=40Mhz,帧时钟FCO等于采样速率10Mhz。我在采样的时候用示波器测量发现,DCO和FCO都是正常输出的,分别是40M和10M,而我的数据输出速率却也是10Mhz,这个事情不知道是什么问题?下图依次是DCO、FCO、采样时钟…

  • [AD9287eval board] how to change input drive for DC signal?

    Hello,

    The customer is using AD9287 EVM.

    They would like to measure the signal that mixed DC. But EVM has capacitor for rejecting DC.

    Is there any way to modify EVM input stage for accept DC level signal?

    Thank you for your help as always.

    Best regards…