Hello all,
I am currently looking for a evaluation board for data acquisition. It should contain a high-speed bipolar ADC.
The AD9286 (500 MSps, 8 Bit) seems to hit my requirements. It has a differential input with full scale voltage of 1.2 Vpp. Can…
Hello,
We're trying to implement SPI control for AD9286 using a Virtex 5 FPGA. The data sheet says that FF reg. must be set to 01 for a write operation. We're setting 5 SPI registers. Must this FF<-01 be sent every single time before sending an SPI instruction…
Hi, there
I'm using AD9286 on zynq through FMC interface. Now I want to use spi communication to control AD9286. Here is my problem, when I send a read command to AD9286, for instance, 0x8000, I should receive 0x18 but I receive 0x800000. And I've…
We're using an AD9286 for our DAQ applications. So, we're developing this system as a microblaze system.
Are there any available microblaze based SPI drivers for AD9286 ? If not, can we use some other ADC's SPI driver for this IC also…
Hi, I'm using the AD9286 in a new design and I have a little question about the Vref.
I want to use the SPI comunication to control the Vref. But do you need to put 1V on this pin or the pin need to be NC.
Hi,
I am currently using the AD9286 board. At the moment, I am just trying to measure the output voltage of each binary bit at logic '1' and logic '0'. I was able to measure, using DVM, a voltage of 1.8V for the negative bits (D0- to D7-) and 0.5V for…
Hi all,
I'm trying to do SPI control for the AD9286 High speed ADC using an Arduino Uno and Labview. The outputs from the Arduino Uno are 5V for logic high and 0 for Logic Low. I saw while reviewing the schematic of AD9286-500 BZ (UG191.pdf) that the…
I used AD9286-500EBZ for testing and found that it could use XTAL as clock source. I read the user guide of AD9286 EVB - UG-191. There is part number of Y505 available for optional crystal oscillator clock source. Could you please help offer…
评估板AD9286-500EBZ技术咨询