• CWD IV amplifier driving capability

    Hi,

    In AD9278, using ADA4841 as IV amplifier. But it mention that one ADA4841 has maximum sum number (4 AD9278s, 32 channels). If we use ADA4896 as IV & summing amplifier, how to calculate the number of channel can be summed in one ADA4896? Note that…

  • CWD phase noise

    Is there any 4LO phase noise requirement in Continuous Wave Doppler ultrasound of AD9278 ?

    Thanks.

  • HSC ADC EVALCZ - AD9279 to MATLAB

    Hi,

    I am trying to use the HSC-ADC-EVALCZ and AD9279 to send data directly to MATLAB. As per the other forum: https://ez.analog.com/data_converters/high-speed_adcs/f/q-a/21394/hsc-adc-evaldz-and-matlab, I modified the MATLAB code to be in the directory…

  • 请问超声检测中的AFE的高通滤波器可否屏蔽?

    · AD9272 · AD9273

    · AD9276 · AD9277

    · AD9278 · AD9279

    · AD9670 · AD9671

    需要信号频率1KHz-500KHz,由于存在高通,可能把需要的信号滤除了。

    1可否屏蔽高通滤波器?

    2可否调整到1kHz一下?

  • RE: AD927x: Standby mode and LVDS outputs

    Hello Gym,

    The DCO and FCO outputs are not placed into high impedance mode during Standby mode.  They are kept running. 

    The difference in the Standby power between the AD9278/9 and the AD9272/6 is related to the behavior of the LNA during Standby. 

  • RE: AD9279-65EBZ schematic

    Hi,

    Apologies for delayed response.

    We will be sending on the schematic of AD9279-65EBZ to your email ad.

    I've attached it here as well.

    Regards,

    Meriam

     PDF

  • RE: 签个到,送您好礼啦!(获奖名单已公布)

    深圳,宝安区,我主要做超声设备,最关注ad9675/ad9278,还有adclk846/ad9520

  • I want to port the ML605 LVDS code to Zynq. I only want to use the LVDS data acquisition and not DMA. Please help.

    I am trying to use the AD9278 with Zynq and have downloaded the reference design ML605. I can see that there's a DMA interface in the code. However, I am not able to find SPI interface for configuration, and I have implemented that. 

    I also would…

  • RE: Data capture problem and configuring in AD9279

    Hi Girish,

    VisualAnalog already comes with configured canvases for AD9279 that you can use to display signals in time domain and frequency domain. Please follow the attached document to setup the boards and hopefully you will be able to display signals…