FAQ
AD9277 is designed for ultrasonic applications, it seems that the LNA is designed for single-ended inputs, the IN- pins (LGx) are connected to ground with Clg, only the IN+ pins (LIx) are used.
In my application, I want to interface 8 differential opamps…
Hello.
Recently we purchased AD9277 ADC for one of our projects.
In stage of development we find out some mismatches of technical details and descriptions given in the datasheet of the ADC.
Particularly:
Hi there,
I'm using the AD9277 in an ultrasound application and am wondering about the AAF limitation. It looks like the AD9277 has a 387 kHz lower frequency limit (page 32 of the datasheet here - http://www.analog.com/static/imported-files/data_sheets…
Hello All,
Please help me with this, really appreciate.
I just get AD9277EBZ andCVT-ADC-FMC-INTPZ today, and I have Zedboard in hand. I saw there is a reference design for AD9279 with ML605(http://wiki.analog.com/resources/fpga/xilinx/interposer/ad9279…
· AD9272 · AD9273
· AD9276 · AD9277
· AD9278 · AD9279
· AD9670 · AD9671
需要信号频率1KHz-500KHz,由于存在高通,可能把需要的信号滤除了。
1可否屏蔽高通滤波器?
2可否调整到1kHz一下?
我们需要采集16个通道的超声信号,功能是有可变增益放大功能即可,求推荐ADI公司有现货的评估板方案,谢谢!
UG-001H和UG-016需要的评估板在贸泽上都没有货了,是不是ADI公司出了新产品...