AD9273数据输出引脚采不到正确电压数据,输出数据全部都是0,再帮忙看一下AD9273的电路图配置有没有问题
Hi Sanchogus,
There is no power sequence requirement for AD9273, you can power up the DRVDD, AVDD1, AVDD2 at the same time.
If you want to add the power up sequence, I will recommend you the below solutions.
Only power sequence: ADM1185 is easy to use…
我最近在使用AD9273做超声前端。现遇到几个问题,希望可以得到解答。1、芯片上电后,LO、LOSW偏置电压为1.5V,可是实测发现,LO引脚有2.5V,LOSW引脚为1.5V;2、数据手册上说转换速率为10到50MSPS,可是查阅寄存器设置发现没有改变转换速率的设置,所以想请问是如何改变转换速率的,以及芯片型号后缀的25、40、50MSPS分别代表什么含义?3、再进行SPI编程时,是不是只需要设置值改变的寄存器,那些使用默认值工作的寄存器则不需要做任何设置!
我是通过fpga来控制AD9273的,我fpga的电平是2.5v的,但是9273AD9273的SDIO的输入范围是0-2V,那么请问我应该怎么接,是否需要一个电平转化器,有没有比较简单的方案啊,谢谢。
hello,
关于ADI官网提供的AD9272的BXL文件用Ultra Librarian工具转换出现无footprint错误,且转换后无PCB封装,只有原理图符号。
下载链接地址:https://www.analog.com/cn/design-center/packaging-quality-symbols-footprints/symbols-and-footprints/AD9272.html,详细见附件附图!
AD9272BSVZ-40.BXL、AD9272BSVZRL-40.…
· AD9272 · AD9273
· AD9276 · AD9277
· AD9278 · AD9279
· AD9670 · AD9671
需要信号频率1KHz-500KHz,由于存在高通,可能把需要的信号滤除了。
1可否屏蔽高通滤波器?
2可否调整到1kHz一下?
Hello Marcin,
I hope you have managed to get the data coming out of your AD9674.
I am also testing a new board with two AD9674's and having problems. Having previously developed a product using the AD9273 device, I was hoping the AD9674 was going…