• Usage of AD9266-80EBZ

    I want to use AD9266-80EBZ evaluation board without using HSC-ADC-EVALCZ . Is it possible to use AD9266 evaluation board stand alone. Can I interface output of AD9266 with another FPGA? What are digital output connectors used in AD9266-80EBZ evaluation…

  • ad9266

    Hi,

    I'm designing a digitizer based on AD9266-20. It will be transformer coupled, with a 3rd order differential ellittic filter placed between

    transformer output and adc input (anti-aliasing).

    To correctly design the filter I need to know how to…

  • AD9266 Could i connect DNC pins to high-Z pins?

    Hello! i wanted to use one topology for AD9266 and AD9649 on the different variations. These chips are very similar, except for pins 7-12 AD9266 (DNC - Do not connect), AD9649 (D0 - D5). Could i connect DNC pins AD9266 to high-Z pins FPGA? Do it work?

  • RE: Can we use AD9266-80ebz evaluation board with Basys3 or zybo or zedboard. If yes then what connectors we need to connect digital output of AD-9266-80ebz to interface with any of these boards?

    Dear David,

    I want to use AD9266-80EBZ evaluation board without using HSC-ADC-EVALCZ .

    Is it possible to use AD9266 evaluation board stand alone. Can I interface

    output of AD9266 with another FPGA? What are digital output connectors used

    in AD9266…

  • ADS7-V2EBZ for AD9266-80EBZ

    Can I use ADS7-V2EBZ  for AD9266-80EBZ  to evaluate AD9266?

    If yes, do I need to EVAL-ADC-FMC-INT to connect ?

    Does VisualAnalog have linux version?

  • RE: AD9266 eval board schematics

    Hi Cien,

    Thank you for your interest in AD9266.

    • The ADA4937 is not installed on the default board.
    • The AD9266-40EBZ is still available and works with the HSC-ADC-EVALCZ..

    Thank you.

    Doug

  • RE: HSC-ADC-EVALDZ setup issues

    Hi Sujeeva,

    I sincerely apologize for the lateness of this reply.

    I see from the screenshots that the ADC being evaluated is the AD9266. The correct FPGA board for the AD9266 is the HSC-ADC-EVALCZ, rather than the HSC-ADC-EVALDZ as indicated in the…

  • RE: On the output variation of the AD9266

    Hi Yuya-san,

    I've attached files of AD9266 output data with inputs floating.

    One attachment is FFT (noise only).

    One attachment is time domain data (noise only).

    The board I found on my bench was a 40Msps part, so the data is at 40Msps.

    Thanks…

  • RE: the SPI communication issue of AD9266

    Hi,

    Thank you for using the AD9266 in your design.

    When you write to Address 0x08 through Address 0x18 you must write Address 0xFF = 0x01 for the command to take effect.

    Please refer to the "Transfer Register Map" section and descriptions of "0xFF"…

  • RE: Help datasheet CAN AD9266

    Hi-

    I noticed this question about the AD9266 was also posted to the High Speed ADC Community at: Help datasheet CAN AD9266.  Someone there should be able to assist you so I'm locking this thread to avoid duplication of effort.

    Thanks,

    AndyR

    EngineerZone…