• 7z100 with four AD9265, failed with adi axi dmac.

    I have a custom designed zynq 7z100 board,  with four AD9265 chip on it, and I create the hdl as the demo hdl, change the dts file for four channel AD9265. See design_1.pdf.

    For some implemention error, I change the ad9265 ip core, and repackage it, change…

  • AD9265

    Dear Sir/Madam,

    I am using the AD9265 to acquire che digital signal, and I wonder knowing  AD9265 is double edge-triggered or single edge-triggered, could you please help clarify it..

    Thanks.

  • RE: AD9467-FMC-250EBZ clock options

    Hi Idmaze,

    The ad9265-fmc-125ebz board has some commen points with mine.The default clock path is the external clock. And you can reference AD9265 Native FMC Card Reference Design [Analog Devices Wiki]

    The ad9265 will be drived by the default clock…

  • HOW I get source code of AD9265 for FPGA on High Speed ADCevaluation board?

  • RE: AD9467-FMC-250EBZ Xilinx Reference Design

    Dear Istvan,

    thank you very much for your support.

    I have another question. For my project, we might move to the AD9265-FMC-125EBZ (I know there are no Reference Design for Zed(Pico)board). The reason is that, if I'm not mistaken, the minimum sampling…

  • RE: AD9265-FMC missing SDK sw

    Dragos,

     

    Per your instructions, I have created a bootable SD image, booted the Zedboard with the AD9265-FMC-125EBZ mounted on it.  I then ran the 'ADI Update Tools' and 'ADI Update Boot' programs.  As you indicated, '/media/analog/BOOT…

  • RE: adi-ad9265-fmc-125ebz.dtsi file seems to be missing from most recent SD card image

    Here is the answer:

    1) Yes the .dtsi files are controlled by the Linux repository.

    2) When they are committed, they are committed to this location:  linux/arch/arm/boot/dts

    3) Branch 2014_R2 has the required file adi-ad9265-fmc-125ebz.dtsi, though…

  • AD9265的使用

    我选用了AD9265采集数字信号。AD9265的时序图见上图。请问AD9265采用的是双边沿输入,单边沿输出么?能不能详细的描述一下?

    哪位大侠指点一下?谢谢!

  • RE: Verilog/VHDL for AD9265 Configuration via SPI

    Hello Wayne,

    We don't have a reference design with the use case you have in mind, for any of our projects at this time.

    We have an HDL reference design for AD9265 FMC at https://github.com/analogdevicesinc/hdl/tree/master/projects/ad9265_fmc which works…

  • AD9269 chip linux driver and axi_dmac

    Hi,

    I have a custom designed zynq board (the schematic is copied from ZC706), with a single AD9269 chip on it,

    but without a AD9517 chip, AND, AD9269 has not a corresponding driver in linux kernel!

    I want to use axi_dmac to send ad9269 sampled data…