• Questions on AD9262

    Hi,

    I have some questions the ADC AD9262

    1.  In the data sheet, on page 24, it says "When 3.3 V voltage levels are  desirable, the DRVDD power supply must be set to 3.3 V. " It looks to me  like that when the DRVDD is 3.3V, all the digital output…

  • How to clock the AD9262 Evaluation board?

    Hi,

    I have a AD9262 evaluation board with Data Capture kit HSC-ADC-EVLAC.

    I am trying to use a DG2020A a data generator to provide an external clock source (80MHz) to the AD9516 using the PLL. Is there some procedure that I can do this? How should…

  • Drivers to Communicate [ AD9262 + HSC-ADC-EVALC ] with third party software eg: NI LabView  etc.

    Hello ,

             I have a AD9262 and HSC-ADC_EVALC data capture board , I would like to use a Third party instrument control software ( LabView ) to communicate to these two. I want to know how I can get the driver modules to successfully interface them.

  • Substituting ADL5387 for ADL5382 in CN-0062

    If ADL5387 is substituted for ADL5382 in CN-0062, can resistor RCM be used to set common mode input voltage for AD9262 ADC?

    Does the 91mA current also apply to ADL5387?

    Is this assumption with the BIAS pin (pin3) left open or with an Rbias resistor…

  • Best Pairings of Mod+DAC and Demod+ADC

    Are there recommended pairings of ADI modulators and DACs and demodulators and ADCs to get the best performance?  I had called in to tech support and they had recommended the ADL5375 and ADL5380.  Circuit Notes CN0021 and CN0062 recommend AD9783/AD9788…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • 工程师百问百答系列之——软件无线电

    上个月,咱们亚洲技术支持中心的同事在媒体网站上举办了“集成式软件无线电”的主题研讨会。软件定义无线电,这个很“高富帅”的主题很是吸引了大家的关注,这里整理出有代表性的技术问答与大家分享。也欢迎大家就软件无线电相关话题提出您的问题哦(咱们亚洲技术支持中心的专家论坛坐镇支持哟)^_^

    本研讨会介绍将RF到基带的高速模拟信号链与FPGA数字信号处理相结合,可用于无线通信。话题涉及高速模拟信号链、直接变频无线电架构、高速数据转换器接口以及软件定义无线电中的FPGA数字信号处理。演示使用新一代的模拟器件高速数据转换器…

  • 软件无线电技术百问百答

    咱们专家在媒体论坛中举办了“集成式软件定义无线电”的技术讲座,介绍了将RF到基带的高速模拟信号链与FPGA数字信号处理相结合,可用于无线通信。话题涉及高速模拟信号链、直接变频无线电架构、高速数据转换器接口以及软件定义无线电中的FPGA数字信号处理。演示使用新一代的模拟器件高速数据转换器、RF和时钟器件以及Xilinx Zynq-7000 SoC。其它话题包括调制器/解调器导致的系统问题,特别是温度和频率变化造成的影响。探讨可以减少这类问题影响的工厂和现场算法,尤其是一劳永逸的工厂预制算法。(…