• AD9262 How to solve start-up trouble

    Do I have to consider anything special at start-up?

     

    The reason for trouble at start-up can be because the digital comes up at an
    unknown state if the clock is not applied before the power supply. 

    To prevent this trouble, you can apply a digital…

  • [AD9262] ADC Stop during operation

    Hello?
    Thanks in advance for my question.
    I use the AD9262.
    Use according to the guidelines (Table 9.).
    The chip ID reads 0x22 well through SPI, and the value I set is well written and read.
    CLK uses 52MHz, MUX uses 25, and KMOD uses 13 to generate a DCO of…

  • RE: AD9262 configuration example

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD9262 unused pins

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: can I control the AD9262 with a HSC-ADC-EVALCZ in Win7 64bit OS with Labview?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD9262/AD9267 Replacement

    Hi,

    AD9262/AD9267 are not recommended for new designs with no replacements proposal. What would you recommend as CTSD ADC with similar performance?

    Regards,

    Ivan

  • AD9262 Synchronization

    Is there any way to synchronize multiple AD9262's for phase coherent operation across multiple parts?

  • RE: AD9262 SPI programming

    Hi PMH,

    Due to a project changes, this project was suspended. Now it comes back to life. I again take the development responsibility. With regard to my last post, is there anything wrong with the configuration sequence I listed? The symptom is still…

  • Image Rejection and QEC of AD9262

    Hi,

    The application is an Ultra Wide-Band Direct Conversion Receiver (400MHz-6GHz) for a Spectrum Analyzer utilizing the ADL5380 and AD9262.

    The datasheet for ADL5380 states it's Image Rejection (worst-case) is -46 dB @ 3.6GHz.

    1) I am interested…