Hello
Can I use Eval-AD9259 with AD-ADC-FMC Adapter Board (EVAL-ADC-FMC-INT)?
If no, can you suggest other solution to connect AD9259 to FMC connector?
Thank you
Hi,
I want to use the quad ADC AD9259 for an imaging application, which requires high DC accuracy and low noise across the whole ADC input range. Reading the datasheet, the maximum (and recommended) input range is 2V peak-to-peak, which is above the…
我正在学习如何给ADC写FPGA的驱动,想写SPI控制模式,学生党缺乏开发项目经验,想要参考一下的AD9259芯片的Verilog代码驱动学习一下。希望可以有人帮助我,非常感谢!
我想用AD9259芯片做ADC采集电压数据,自己没有多少工程经验写不出来这个代码,有没有做过的的可以给个源代码参考一下呢
我想用AD9259芯片采集电压数据,自己没有多少工程经验写不出来这个代码,有没有做过的的可以给个源代码参考一下呢,
My customer needs four channels, 12 bit min (14 or 16 would be better), 50MSPS ADC solution, looking for Linux drivers to use with ZC706. A single ADC would work, but if we have a solution that used two dual ADCs, that would be fine too.
I'm looking at…
I'm using IBIS AMI model of ad9250 supplied by Analog (AD9250 AMI Model (Rev. 1.2) in ANSYS Electronics Desktop. In Electronics Desktop I loaded the model, but during VeriEye analysis I encountered the following error.
It seems that the model…
I'm using IBIS AMI model of ad9250 supplied by Analog (AD9250 AMI Model (Rev. 1.2) in ANSYS Electronics Desktop. In Electronics Desktop I loaded the model, but during VeriEye analysis I encountered the following error: