• RE: AD9249 design resources

    Hi Richard,

    I've placed the Cadence layout file of the AD9249 evaluation board ( 08_039099b.brd ) into the zipped layout files archive on the Wiki site (same link as previously stated above: https://wiki.analog.com/_media/resources/eval/ad9249_fmc_brd_designfiles…

  • ad9249 Design resources

    hi i am student . i need vhdl code of ad9249 that i use chip in my project .

    thanks analog devices

  • RE: AD9249 Evaluation Board: clock (CLK+) frequency issues

    Hi,

    I'm sorry about the confusion.

    As stated in Table 4 of the AD9249 datasheet, the minimum sample rate of AD9249 is 10Msps, so 10.8333M is above the minimum and so it is OK.

    Register 0x100 sets AD9249 into lower power states with new maximum (not…

  • RE: AD9249 frame and data clock source

    Hi,

    thank you for your answer.


    I am referring to the one on the evaluation board, M24C02-WMN6TP on page 4 of the evaluation board's schematics.


    In general, we are not sure which purpose the pins C30-C40 and D30-D40 in the FMC connector serve and cannot…

  • AD9249-65EBZ

    I have the AD9249-65EBZ board. I do not have any of the recommended interfacing boards. I have powered the board with 6V and removed the jumpers on P1. I have attached connections to a micro-controller to the middle pins 2, 5, 8, 11. I then attempt to…

  • Application questions about AD9249

    Hi,

    I want to design a 10-channel data acquisition circuit with AD9249. There are two quesions:

    1、AD9249 has 16-channel. What should I do with the unused analog input VIN− and VIN+? Tied to GND, or just left floating?

    2、What should I do with the…

  • AD9249 aperture delay variation

    Hi
    In AD9249 datasheet I can find the following aperture related specs:
    - Aperture Delay
    - Aperture Uncertainty (Jitter)

    But I can't find anywhere  "Aperture mismatch within device" or "Aperture delay variation Channel-to-channel within the same device…

  • Interfacing AD9249 with FPGA

    Hello everyone,

    for my project I am using the board AD9249-65EBZ with an FMC connector. The 14-bit LVDS data is supposed to be sent to a Xilinx Zynq 7000 ZC702.

    Having a look on the reference designs from Xilinx, this is not a straight forward task,…

  • AD9249: FMC connector

    Hi,
    In the project I'm working on, a connection must be made between a zynq ZC702 (Xilinx Zynq-7000 SoC ZC702 Evaluation Kit, www.xilinx.com/.../ek-z7-zc702-g.html) and an analog devices board AD9249 (www.analog.com/.../EVAL-AD9249.html. To test the…

  • AD9249 Evaluation Board

    Hello. I have an question to the following product: AD9249 Evaluation Board.

     

    (1) Is the source code (VHDL) freely available? (Download-Link ...)

    (2) I have currently the HSC-ADC-EVALCZ. Can I use the AD9249 Evaluation Board at this without probl…