FAQ
is ad9248 available or obsolete and also can you suggest the adc similar to it and its datasheet
查看AD9248的手册,电气特性中似乎并没有标注模拟输入电压范围,只写了电压跨度(个人猜测应该是说的差分输入的跨度)。AD9248的VIN+A、VIN-A等对地的输入电压范围到底是多少?虽然绝对最大额定值里面有写,输入的安全范围应该是多少?
can anyone provide the AD9248BCP-65EBZ orcad schematic design file ?
otherwise kindly provide AD9248 LFCSP , orcad design symbol .
Hello
I have a 100mVp-p signal and the frequency range is between 100KHz to 10MHz.
the AD9248 has some Reference configuration to select Vref (it could be 0.5V or 1V).
*if I want to sample the signal with AD9248, which voltage reference is better to…
Does anyone have an AD9248 evaluation board I could get from them ?
关于AD9248的时序:
你好:
在AD9248的我看的是一头雾水。问题如下:
1.我需要时序图,截屏或其它手册可以看到,或其它芯片可以参考也可以。
2.由于项目的需要,我需将芯片设置成并口进CPLD,如何设置?
3.芯片乘法是不是一个时钟,AB是同时给出,谁高谁低?
4.那个公司可以提供评估板学习一下准确的时序,谢谢?